Arduino
  • Products
  • More
Arduino
Arduino Forum Pull-up resistor on bread board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 1298 views
  • Users 0 members are here
Related

Pull-up resistor on bread board

e14 Contributor
e14 Contributor over 14 years ago

Hi,

I'm new to the designing circuits.  I would like to connect two Waterproof DS18B20 Digital temperature sensors and measure the difference. http://www.adafruit.com/products/381  I understand the concept of the bread board, but I'm having trouble visualizing setting up the pullup resistor pictured here: imagehttp://www.hacktronics.com/images/arduino_ds18b20_connection.jpg

 

 

 

 

I would usually expriment with something like this on my own, but there was a waring that said if wired wrong could fry the board.....and I just got it image

 

 

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Wow that was quick...thanks for the fast and accurate answers!  I now have the first sensor connected and gving me back data image 

     

    my sensor is the waterproof kind, but the withe the description your provide and the pic it was easy to do.

     

    Now I need to add a 2nd sensor to the board....since it a single line bus I can I connect the power, ground, and data lines on the same rows or do I have to something special that I use two resistors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Wow that was quick...thanks for the fast and accurate answers!  I now have the first sensor connected and gving me back data image 

     

    my sensor is the waterproof kind, but the withe the description your provide and the pic it was easy to do.

     

    Now I need to add a 2nd sensor to the board....since it a single line bus I can I connect the power, ground, and data lines on the same rows or do I have to something special that I use two resistors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    The one resistor is a pull-up for the entire bus so no extra resistor is needed.

    Just put the second one on the same row as the previous one and you're good to go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer