Arduino
  • Products
  • More
Arduino
Arduino Forum A quick question
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 417 subscribers
  • Views 338 views
  • Users 0 members are here
  • wheel
  • pot
  • teensy
  • steering
  • arduino
Related

A quick question

dirtdiver
dirtdiver over 13 years ago

Hi everyone,

i was wondering if i can get readings from one potentiometer on two separate devices- like in my case a teensy and a USB PC steering wheel?

i was considering diods or pots twise the resistance they were but im not really sure what would be correct

Any help is appreciated

  • Sign in to reply
  • Cancel
  • evan.stoddard
    0 evan.stoddard over 13 years ago

    Im sorry, can u explain a bit more.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to evan.stoddard

    DirtDriver

    The short answer is yes.

     

    If the potentiometer produces a voltage, (it will be connected to the +ve rail and ground) then you could split it via two resistors to each device.

    This is probably going to impact on both circuits, and both devices need to run on the same voltage and have their ground pins tied together.

     

    The easier way is to use dual potentiometer. These have a single shaft and two seperate variable resistance elements.

    Both devices will be isolated from each other.

     

    A quick check shows a number of types with varying prices.

     

    Hope this helps

    Mark