Arduino
  • Products
  • More
Arduino
Arduino Forum What is your opinion of Galago (Arduino compatible Kickstarter Project) ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 1089 views
  • Users 0 members are here
  • arduino_compatible
  • arduino_alternative
  • arduino
Related

What is your opinion of Galago (Arduino compatible Kickstarter Project) ?

JRR
JRR over 13 years ago

Hi,

 

I'd like to know what is your opinion to the Galago project (ongoing) on Kickstarter?  How do you think it compares to the Teensy Project (already over).

 

Thanks in advance,

 

JRR

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to JRR +1 verified
    I designed Galago, so perhaps I can answer your question. The NXP chip we use is has a 50% faster top clock speed than the Teensy's Freescale chip. It's also widely believed that the Teensy's Cortex-M4…
Parents
  • mlass
    0 mlass over 13 years ago

    http://www.electronicsweekly.com/Articles/22/02/2010/48047/arm-adds-dsp-in-cortex-m4-core.htm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • JRR
    0 JRR over 13 years ago in reply to mlass

    The Teensy has an M4 while Galago has an M3.  According to the article (thanks for the link), Galago is not as powerful as Teensy.

     

    - If it is intended to replace typical Arduino like applications will the lesser M3 be enough?

    - Is the Teensy's longer development history (more projects available) make a difference?

    - Is the debugging feature of the Galago worth it? Enough to overcome the previous two?

    - Can Teensy come up with a debugging scheme, or is it somehow built into the galago?

     

    Thanks in advance

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to JRR

    I designed Galago, so perhaps I can answer your question.  The NXP chip we use is has a 50% faster top clock speed than the Teensy's Freescale chip.  It's also widely believed that the Teensy's Cortex-M4 has a floating-point unit but this is not the case - it only has integer vector extensions which must be specifically coded for, like MMX on the Pentium.  Our M3's capabilities also outlcass the Arduino in every regard and its built-in debugger is unmatched compared to what's possible on AVR-based boards like the Arduino.  Finally, there's no possibility of debugging the Teensy 3.0 - Paul Stoffregen stated that the JTAG pins are not broken out on his board, so even an external debugger isn't an option.

     

    I hope this was helpful info!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • fustini
    0 fustini over 13 years ago in reply to e14 Contributor

    Happy to see you posting here, Kuy.  I backed the Teensy 3.0 a couple weeks ago as I was excited about the prospect of using Arduino on ARM (and unsure of the DUE roadmap).  I noticed on the Galago page states C, C++ and Wiring.  Could you comment as to how similar the process of developing with Wiring on the Galago will be to AVR-based Arduino?

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to fustini

    Certainly. We're implementing this with a thin layer on top of our normal API that provides compatibility with Arduino/Wiring API functions like digitalRead() etc.  For marketing literature brevity and in the absence of a formal standard we call this Wiring compatibility, though we may need approval or buy-in from the Wiring copyright holders to state that officially.

     

    Going forward, we intend the aforementioned compatibility layer to act more as a bridge for Arduino users than a long-term platform because we believe our API is better-designed, more usable and will lead to ultimately better projects.  Obviously whether that turns out remains to be seen after release.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mlass
    0 mlass over 13 years ago in reply to e14 Contributor

    Thanks for the info.  I'm also a backer of the Teensy 3.0, but just joined the Galago Starter Kit and can't wait to compare the two.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mlass
    0 mlass over 13 years ago in reply to e14 Contributor

    Thanks for the info.  I'm also a backer of the Teensy 3.0, but just joined the Galago Starter Kit and can't wait to compare the two.