Arduino
  • Products
  • More
Arduino
Arduino Forum Interfacing Ps2(playstation) with Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 540 views
  • Users 0 members are here
Related

Interfacing Ps2(playstation) with Arduino

e14 Contributor
e14 Contributor over 13 years ago

Hey I am interfacing Ps2 with an arduino to control servo motor wirelessly.My code is able to detect ps2 but it's not reading input from ps2.please tell me Is there any problem in my code.Here is my code::image

 

#include <Servo.h>

#include <PS2X_lib.h>

 

 

Servo myservo;

PS2X ps2x;

int ps2x_error = 0;

byte ps2x_type = 0;

byte ps2x_vibrate = 0;

 

 

int pos = 0;// variable to store the servo position

const byte servoPin = 9;

byte incomingByte;

 

 

void setup()

{

  {

  Serial.begin(9600);

  myservo.attach(9);  // attaches the servo on pin 9 to the servo object

  pinMode(servoPin, OUTPUT);   

  }

  

   

  ps2x_error = ps2x.config_gamepad(13,10,11,12, false, false);

 

 

  if(ps2x_error == 0)

    Serial.println("Found Controller, configured successful");

  else if(ps2x_error == 1)

    Serial.println("No controller found, check wiring.");

  else if(ps2x_error == 2)

    Serial.println("Controller found but not accepting commands.");

  else if(ps2x_error == 3)

    Serial.println("Controller refusing to enter Pressures mode, may not support it. ");

   

   

 

 

  // get which type

  ps2x_type = ps2x.readType();

  switch(ps2x_type)

  {

  case 0: Serial.println("Unknown Controller type");  break;

  case 1: Serial.println("DualShock Controller Found");  break;

  }

}

void loop () {

  if((ps2x_error == 1) || (ps2x_error == 2) || (ps2x_error == 3))

    {

    //skip loop if no controller found

    return;

     }

  else if(ps2x_error == 0)

  {

    if(ps2x_type == 1)

    {

     

     

   ps2x.read_gamepad(); //read controller

 

 

    if(ps2x.Button(PSB_PAD_UP))

      {    

        Serial.println("Up ");

        for(pos = 0; pos < 90; pos += 1)  // goes from 0 degrees to 180 degrees

  {                                  // in steps of 1 degree

        myservo.write(pos);              // tell servo to go to position in variable 'pos'

        delay(15);                       // waits 15ms for the servo to reach the position

  }

       

      }

      else

      {

        Serial.println("DOWN ");

         for(pos = 90; pos>=1; pos-=1)     // goes from 180 degrees to 0 degrees

  {                               

         myservo.write(pos);              // tell servo to go to position in variable 'pos'

         delay(15);                       // waits 15ms for the servo to reach the position

  }

      }    

     

    

   

     

   

}

  }

  delay(50);

}

  • Sign in to reply
  • Cancel
  • t0mpr1c3
    0 t0mpr1c3 over 13 years ago

    I had exactly the same issue connecting a Guitar Hero whammy pedal to a servo. My guess is that the bitbanged serial communication with the PS controller is incompatible with the software PWM used in the Servo library. Try the old hardware PWM library instead: http://arduiniana.org/libraries/pwmservo/