Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino and phpmyadmin
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 416 subscribers
  • Views 711 views
  • Users 0 members are here
Related

Arduino and phpmyadmin

e14 Contributor
e14 Contributor over 13 years ago

Hi guys. I am new to arduino and i want to make a project for my university, using Temperature Sensors and uploading the results to phpMyadmin. I am checking everywhere to find a solution but i have totally "crushed"!!!

The problem is that while it seems to be a connection between arduino sketch and phpMyadmin in my database fields, the sketch returns only 0.00 and i can't find the problem. I thank you all in advance. Every possible answer is thankfully accepted.

 

 

This is the part of Arduino sketch that transfers data to my database

 

void loop(void)                                        

{

if(!connected)   {                                              

//Serial.println("Not connected");


if (client.connect(serverip,80)){         

sensors.requestTemperatures();          // send the request for temperature to sensors



float temp1 = sensors.getTempCByIndex(0);    


// take temp reading from sensor "i" and store it to temp1


Serial.print("Temp is ");                               

Serial.println(temp1);

Serial.println("Sending to Server: ");                   

client.print("GET /mysql_connect.php?temp1=");       

Serial.print("GET /mysql_connect.php?temp1=");           

client.print(temp1);

Serial.print(temp1);

client.println(" HTTP/1.0");                 

Serial.println(" HTTP/1.0");                 

client.println();                            

Serial.println();

delay(20000);                                            // send the temperature every 20 sec

}

 

 

This is my mysql_connect.php file

 

<?php


if (isset($_GET['temp1']))

{

$temp1 = floatval ('temp1');

$temp1 = $_GET['temp1'];




$con = mysql_connect("host","username","password");

if (!$con)

   {

   die('could not connect: ' .mysql_error());

   }

  

mysql_select_db("temp_database", $con);


$sql="INSERT INTO temperatures (temp1) VALUES ($temp1)";


echo "inserted correctly \n";


if (!mysql_query($sql,$con))

   {

   die('Error: ' . mysql_error());

   }

  

if (mysql_query($sql,$con)){  

echo "1 record added";

}

mysql_close($con);

}

?>

 

 

In this part of my php code:

 

$sql="INSERT INTO temperatures (temp1) VALUES ($temp1)";

 

when i just put a random float (e.g. 42.05) it works perfectly, but when i leave it just like above and "expect the communication" between Arduino and php i have the problem. I type in my browser:

 

localhost/mysql_connect.php?temp1=

 

And the message i get is:

 

Error: Column count doesn't match value count at row 1

 



  • Sign in to reply
  • Cancel
Parents
  • ntewinkel
    0 ntewinkel over 13 years ago

    I wonder about these 2 lines:

     

    "

    $temp1 = floatval ('temp1');

    $temp1 = $_GET['temp1'];

    "

     

    The second line overwrites the float value obtained by the first, doesn't it?

     

    Can you test the script by pointing a browser directly at it and then typing in what the Arduino would be sending?

     

    Also, in the Arduino code, should this be a println rather than a print?

    "

    client.print(temp1);

    "

     

    And is this line needed?

    "

    client.println(" HTTP/1.0");

    "

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 13 years ago

    I wonder about these 2 lines:

     

    "

    $temp1 = floatval ('temp1');

    $temp1 = $_GET['temp1'];

    "

     

    The second line overwrites the float value obtained by the first, doesn't it?

     

    Can you test the script by pointing a browser directly at it and then typing in what the Arduino would be sending?

     

    Also, in the Arduino code, should this be a println rather than a print?

    "

    client.print(temp1);

    "

     

    And is this line needed?

    "

    client.println(" HTTP/1.0");

    "

     

    Cheers,

    -Nico