Arduino
  • Products
  • More
Arduino
Arduino Forum Python to Arduino to Motors...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 417 subscribers
  • Views 3164 views
  • Users 0 members are here
  • freetronics
  • immediate
  • raspberry
  • c
  • python
  • help
  • pi
  • pwm
  • support
  • control
  • rasppi
  • rpi
  • c++
  • motor
  • arduino
  • varible
Related

Python to Arduino to Motors...

wallarug
wallarug over 13 years ago

I have two reversable 12volt motors that I would like to control through PWM.  I want the speed to be constantly updated by the python code that will be sent through a TCP client-server.  I have the python piece of code working very well. I need some help with the Arduino Sketch please.  I have all the other pieces of code working except the Arduino Sketch.

 

I know everything about the hardware required (H-bridge, etc) but I need help with the sketch.

 

 

This is the Joystick Control and TCP client:

 

 

[code]import pygame

import socket

import sys

import os

pygame.init()

j = pygame.joystick.Joystick(0)

j.init()

 

print 'Initialized Joystick : %s' % j.get_name()

username = os.name

if username == "nt":

    username = "Windows"

print "Welcome commander, you are using " + username

 

 

 

 

a = 0

b = 0

aa = a

bb = b

 

 

 

 

 

 

 

 

i = raw_input("What do you want to detect?")

while i == "button":

    pygame.event.pump()

    #print j.get_axis(1)

    if j.get_button(1):

        print "Left"

    if j.get_button(0):

        print "Kill"

    if j.get_button(2):

        print "Right"

while i == "pos":

    pygame.event.pump()

    y = j.get_axis(1)   ######################################

    y = round(y,2)      # Increase to (x, 12) when using PWM!#

    x = j.get_axis(0)   #  @@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@   #

    x = round(x,2)      # Increase to (y, 12) when using PWM!#

    z = j.get_axis(2)   ######################################

    z = round(z,1)

    #print(x,y,z)

  

    if y < 0:          ############################

        y = abs(y)     #New Y-axes inversion code!#

    elif y > 0:        ############################

        y = y*-1

 

 

#############################################

# Formulas for working out the speed of the #

# motor in certain areas of the Joystick!   #

#############################################

 

 

    f = 1

    sy = f*(y)

    sx = f*(x)

   

 

 

#############################################

## Whenever the ROBOT is moving and the     #

##  Co-ordinates are not (0,0)              #

#############################################

 

 

                               

    if x != 0 and y != 0:      

        sy = abs(sy)                    #######

        if y > abs(x) and y > 0:        # Top!#

                                        ############

            if -1 < x < 0:              # Top Left!#

                                        ############################################

                c = abs(x)              # Convert to percentage and positive value!#

                a = (sy) - (c)          ############################################

                b = (sy)

                                        #############

            elif 0 < x < 1:             # Top Right!#

                                        ############################################

                d = abs(x)              # Convert to percentage and positive value!#

                b = (sy) - (d)          ############################################

                a = (sy)

            else:

                a = abs(x)

                b = abs(x)

 

 

                                        ##########

        elif y < -abs(x) and y < 0:     # Bottom!#

                                        ###############

            if -1 < x < 0:              # Bottom Left!#

                                        ############################################

                c = abs(x)              # Convert to percentage and positive value!#

                a = (sy) - (c)          ############################################

                b = (sy)

                                        ################

            elif 0 < x < 1:             # Bottom Right!#

                                        ############################################

                d = abs(x)              # Convert to percentage and positive value!#

                b = (sy) - (d)          ############################################

                a = (sy)

            else:                       ############################################

                a = abs(sy)             # So that values "a" and "b" are regonised #

                b = abs(sy)             #  by python reader (I had problems)!      #

                                        ############################################

 

 

 

 

                                           

#################################

# Special formula for when you  #

#   leave the "allowed" area    #

#################################

 

 

        elif y < abs(x) and y > -abs(x): 

            if x < 0:

                b = abs(x)

                a = 0

            elif x > 0:

                a = abs(x)

                b = 0

            else:

                a = 0

                b = 0

 

 

 

 

 

 

##################################

# Special Formula for all values #

#  on the x-axis for immediate   #

#    turning.                    #

##################################

 

 

    elif y == 0:

        if x < 0:

            a = 0

            b = abs(sx)

        elif x > 0:

            a = abs(sx)

            b = 0

        else:

            a = 0

            b = 0

 

 

 

 

 

 

#######################################

#  Anything else that is not defined  #

#   (Only when x and y = 0)           #

#######################################

 

 

    elif x == 0:

        a = abs(sy)

        b = abs(sy)

 

 

    else:

        a = 0

        b = 0

       

              

 

 

######################################

### PWM convetion for AnalogueWrite()#

######################################

 

 

    PWM = 255

    a = PWM*a

    a = round(a,0)

    a = int(a)

    b = PWM*b

    b = round(b,0)

    b = int(b)

 

 

 

 

 

 

 

 

####################################

# Printing Output - Only used in   #

# development of Joystick Control. #

####################################

 

 

    #print (a,b)

 

 

########################

# TCP client is below. #

########################

 

 

    data = (a,b)

    HOST, PORT = "192.168.12.12", 9999

    #HOST2, PORT2 = "10.88.112.174", 9998 # Change to server when necessary

    sock = socket.socket(socket.AF_INET, socket.SOCK_STREAM)

    sock.connect((HOST, PORT))              ## CIAN HAS CHANGED!!##

    ##sock.sendall(str(data) + "\n")

    ##print "Sent:     {}".format(data)

 

 

    if a != aa or b != bb:

        sock.sendall(str(data) + "\n")

        print "Sent:     {}".format(data)

##    elif a == aa and :

##        print (int(a),int(b))

 

 

    aa = a

    bb = b

 

 

 

 

#####################################################

##@@@@@@@@@@@@@@@@@@@@@@ END @@@@@@@@@@@@@@@@@@@@@ ##

#####################################################[/code]

 

 

This seems to work ok, I am working on getting the TCP Client quicker - so that is a bit of a mess right here.

 

 

This is how far I have gotten with the Arduino Sketch:

 

 

[code]/*

* Robot Motor Controller script with PWM speed control

*/

//---------------------- Motors

int motorL[] = {6, 7};

int motorR[] = {8, 9};

int ledPin = 13;

int motor_a = 0;

int motor_b = 0;

int dir_y = 5;

 

 

 

 

void setup() {

Serial.begin(9600);

int i;

for(i = 0; i < 2; i++){

pinMode(motorL[i], OUTPUT);

pinMode(motorR[i], OUTPUT);

pinMode(ledPin, OUTPUT);

}

 

 

}

 

 

void loop() {

drive_forward(); {

digitalWrite(motorL[0], HIGH);

digitalWrite(motorL[1], LOW);

digitalWrite(motorR[0], HIGH);

digitalWrite(motorR[1], LOW);

analogWrite(9, motor_a);

analogWrite(6, motor_b);

}

drive_backwards(); {

digitalWrite(motorL[0], LOW);

digitalWrite(motorL[1], HIGH);

digitalWrite(motorR[0], LOW);

digitalWrite(motorR[1], HIGH);

analogWrite(9, motor_a);

analogWrite(6, motor_b);

}

}

 

 

void if(y < 0) drive_foreward()

 

 

void if(y > 0) drive_backwards()[/code]

 

 

No surprise that it doesn't work.  I want it to read three values from the Python script which are the speed of the left motor (defined as "a"), speed of the right motor (defined as "b"), direction of motor (which is defined as "y" - when it is <0 it goes backwards or >0 goes forward).

 

 

For the [b]varying speed controls[/b], I will be using PWM (values between 0 -> 255) which uses the "analogWrite(Pin, value)" Syntax.  These values will be changing via the "a" and "b" values from the python script.

 

 

Is there anyway that you can help me with this.  I am really struggling.

 

 

Thanks in advance to anyone who can help.

  • Sign in to reply
  • Cancel
Parents
  • evan.stoddard
    0 evan.stoddard over 13 years ago

    Honestly I'm not totally sure, I don't have any servos and don't have time for a tcp server.  I'm assuming so as long as your variables are the same. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 13 years ago in reply to evan.stoddard

    Thanks for your help so far.  I am going to have a go importing varibles now and see what happens.  I have to find some LEDs to test it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • evan.stoddard
    0 evan.stoddard over 13 years ago in reply to wallarug

    Good luck! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 13 years ago in reply to evan.stoddard

    I need to set the PWM frequency on my Ardunio to 65000Hz.  I am using PWM pins 5 and 6 (which is a good start) but I can't seem to find a conclusive way to increase the clock to that frequency.  Help please.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • evan.stoddard
    0 evan.stoddard over 13 years ago in reply to wallarug

    www.arduino.cc/playground/Code/PwmFrequency. Come on dude use your googlefu ;)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 13 years ago in reply to evan.stoddard

    I was on that page when I wrote the previous post.  I tried that in IDE but that did not work.  The setPwmFrequency(#, #) does not work.

     

    EDIT:

     

    I am using Pins (6, 11) and Pins (5, 3) becasue the PWM did not work when the channels were set to LOW.

     

    The 'Clock' of Channels 6 and 5 are the same (so I have discovered).

     

    I am using LEDs to test the code and PWM.  I think this could be the problem.  The LEDs don't want to 'dim'.  I have the same problem when I am running light shows durring musicals.  I think I will test with some transistors and motors later, they might respond better to the PWM.

     

    BTW: Can you send the PWM directly to the motors?  From what I know, it is just turning a switch on and off very very fast and the Interpting of the singnal is done by the Ardunio ATMEGA.

              Can you confirm this information?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wallarug
    0 wallarug over 13 years ago in reply to evan.stoddard

    I was on that page when I wrote the previous post.  I tried that in IDE but that did not work.  The setPwmFrequency(#, #) does not work.

     

    EDIT:

     

    I am using Pins (6, 11) and Pins (5, 3) becasue the PWM did not work when the channels were set to LOW.

     

    The 'Clock' of Channels 6 and 5 are the same (so I have discovered).

     

    I am using LEDs to test the code and PWM.  I think this could be the problem.  The LEDs don't want to 'dim'.  I have the same problem when I am running light shows durring musicals.  I think I will test with some transistors and motors later, they might respond better to the PWM.

     

    BTW: Can you send the PWM directly to the motors?  From what I know, it is just turning a switch on and off very very fast and the Interpting of the singnal is done by the Ardunio ATMEGA.

              Can you confirm this information?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • evan.stoddard
    0 evan.stoddard over 13 years ago in reply to wallarug

    Where did you put it.  In the loop or set up

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wallarug
    0 wallarug over 13 years ago in reply to evan.stoddard

    /*

    * Robot Motor Controller script with PWM speed control

    */

    //---------------------- Motors

    int motorL[] = {3, 5};

    int motorR[] = {11, 6};

    int ledPin = 13;

    int Byte1 = 0;  //for incoming serial data

    int Byte2 = 0;  //for incoming serial data

    int Byte3 = 0;  //for incoming serial data

    int motor_a = 0;

    int motor_b = 0;

    int dir_y = 0;

    int motor_a_prev = 0;

    int motor_b_prev = 0;

     

     

     

     

    void setup() {

    Serial.begin(9600);  // opens serial port, sets data rate at 9600bps

    int i;

    for(i = 0; i < 2; i++){

    pinMode(motorL[i], OUTPUT);

    pinMode(motorR[i], OUTPUT);

    pinMode(ledPin, OUTPUT);

    }

     

     

    }

     

     

    void loop() {

    digitalWrite(ledPin, HIGH);

     

     

    if(Serial.available()==3)

    {

      Byte1 = Serial.read(); // Incoming data from Serial connection

      motor_a = int(Byte1 & 0x0F);

      Byte2 = Serial.read(); // Incoming data from Serial connection

      motor_b = int(Byte2 & 0x0F);

      Byte3 = Serial.read(); // Incoming data from Serial connection

      dir_y = int(Byte3 & 0x0F);

     

      if (dir_y == 2) { //Motor Backwards

      digitalWrite(motorL[0], HIGH);

      digitalWrite(motorL[1], LOW);

      digitalWrite(motorR[0], HIGH);

      digitalWrite(motorR[1], LOW);

      analogWrite(3, motor_a);

      analogWrite(11, motor_b);

      }

      else if (dir_y == 1) {  //Motor Forwards and Single motor Turning

      digitalWrite(motorL[0], LOW);

      digitalWrite(motorL[1], HIGH);

      digitalWrite(motorR[0], LOW);

      digitalWrite(motorR[1], HIGH);

      analogWrite(5, motor_a);

      analogWrite(6, motor_b);

      }

     

    }

    else: {

     

    }

    Code so far.

     

    I put the command in the Setup()