Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino: open a circuit digitally
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 953 views
  • Users 0 members are here
Related

Arduino: open a circuit digitally

e14 Contributor
e14 Contributor over 13 years ago

hello there. i'm new with arduino but i managed to do some interesting projects. One problem i faced is: I want to build a password keypad in order to open my garage door. My garage door is NOVOPORT and has a circuit so if you connect (open) the circuit it will open (if closed) or close (if open) the garage door. For the moment i have installed a switch (ordinary momentary light switch) so when i click the door is opened or closed.

 

Now back to the problem. I can build a password app in order to turn on a light for example but the problem with the garage door is that im afraid to send 5v current to the motor. So is there any solution to digitally just open a circuit with arduino and not send a 5v power.

 

please help, thx in advance

best regards,

  • Sign in to reply
  • Cancel
Parents
  • mconners
    0 mconners over 13 years ago

    Really what you want to do is replace the momentary switch that you put in place with a digital switch that can be controlled by the arduino. Without knowing the specifics of your application no one will really be able to give you a full answer.

     

    One quick suggestion might be to put a relay in place of your momentary switch and activate the relay using the arduino after the passcode has been properly entered.

     

    Taking the risk of being accused of spamming, something like the following might be what you are looking for:

     

    http://www.amazon.com/SainSmart-2-Channel-Relay-Module-Arduino/dp/B0057OC6D8/ref=wl_it_dp_o_pC_nS_nC?ie=UTF8&colid=M760SG5PMAT8&coliid=I2GQZEOG05XYU1

     

    The parts themselves should be available through your element 14 affilliated retailer if you want to build your own, I just included the link to show the finished item.

     

    Good luck,

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mconners

    Thank you very much for your answer it was veru helpful. I didnt knew anything about relays untill now image.

     

    the project is easy one, which i can implement with a relay very easy. I just open a power circle. make contact between 2 wires.

     

    If there is a possibility to do it digitaly without relays will be better. Any idea?

     

    Let me explain another idea. I want to modify my remote control so the power button requires a password. The arduino is responsible for the password app and has wires connected to the remote board (power button). When a correct code is entered the tv is turned on or of. So i simulate a button press for the remote.

     

    Thank you in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 13 years ago in reply to e14 Contributor

    I think on your first project the relay is the way to go. It's easy and inexpensive. Without looking at a schematic of the whole circuit it would be hard to suggest another way.

     

    As far as the other circuit, with the remote control, you might find it difficult to figure out what the ir code is, but it could be done, if you had the schematic, you might be able to do a similar thing as above, intercept the button press, accept a valid passcode, then bring the line where the button used to go either high or low to match the normal button action, that could be accomplished with an Arduino with little to no external components.

     

    You have some interesting projects. Good luck.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • mconners
    0 mconners over 13 years ago in reply to e14 Contributor

    I think on your first project the relay is the way to go. It's easy and inexpensive. Without looking at a schematic of the whole circuit it would be hard to suggest another way.

     

    As far as the other circuit, with the remote control, you might find it difficult to figure out what the ir code is, but it could be done, if you had the schematic, you might be able to do a similar thing as above, intercept the button press, accept a valid passcode, then bring the line where the button used to go either high or low to match the normal button action, that could be accomplished with an Arduino with little to no external components.

     

    You have some interesting projects. Good luck.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer