Arduino
  • Products
  • More
Arduino
Arduino Forum Help to arduino code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 417 subscribers
  • Views 471 views
  • Users 0 members are here
Related

Help to arduino code

e14 Contributor
e14 Contributor over 13 years ago

Hi. (First I must say that I am from Denmark, so i hope that you understand my english.)

 

I hope that someone will help me. I have tried to make a code for my arduino uno. 

 

I want to have 3 LED's to increase light dependent on a signal from at tempeature sensor.

They should do it in different intervals, so that LED1 should increase light when the signal from the temperature sensor is between 165 and 200, and hold full light to everything above 200.

 

The LED2 should start at 200 and increase up to 225, and hold full light to everuthing above 225.

 

The LED3 should start at 225 and increase up to 240, and hold full light to everuthing above 240.

 

 

 

I have used PWM to control the LED's, but they all light all the time and when the temperature changes they increase and decrease in an uncontrolled way.

 

So my qustions are:

 

1. Why does the LED's light all the time and why do they increase and decrease uncontrolled?

 

As mentioned above, I would like to keep the LED's fully lighted if the value exceeds the limits in the 'if' statement.

 

So second question:

2. Can i in some way use 'constrain' to hold the LED's on when the temperature input signal is over the value that the light should increase on? IF not, what can I use?

 

I have attached the code.

Attachments:
LED_som_funktion_af_temp.ino.zip
  • Sign in to reply
  • Cancel
Parents
  • anhtien
    0 anhtien over 13 years ago

    Jacob,

    1. The code looks better thanks, questions on the current code:

    a. why do you call analogRead twice? I thought you need at least 1ms between reads to get good value.

    b. why do you need to use map etc, you could just do analogWrite(ledx, 0) directly for action a.

    2. The reason for delay of 500ms being too fast: in real life temperature can not change that fast or we are facing end of the world. Let's say you are in a house with this robot you are building and he (or she) has a job of detecting fire.  If there is no fire: green led (or no led on), getting hot: yellow led, red is for the robot being burned.  I believe the right temperature sampling rate would be once every 5 seconds.  Question for you: What do you see on the Serial Monitor screen?  If values change erratically then your sampling is not steady (or something is wrong with the connection).  That would be in conflict with my #3 below.

    3. Assuming you got the sampling steady, there are probably two approaches:

    a.  Each LED goes bright or not (on or off), which is probably what you should start with to make sure your ranges are in good use.

    b.  Getting brighter or dimmer: reading the example "Fade" from Arduino, there is some sort of gradual increase or decrease in value.  Looking at code action c, let's say the sensor reports in the middle range (200 < val < 225), what happen if you have a serie of 200, 210, 202, 225, 215 ?  This is the non-steady situation that the temperature sensor (or pot) might provide, and these values will be spread out (through map function) to 0-255 range.  I believe the LED won't be able to go brighter or dimmer but rather jerking uncontrollably.

    4. Lastly, you might want to try with one LED to see the brightness changes.  Actions b,c,d are for different brightness on 3 LEDS does not seem right, at least looking at the code anyway, try to turn off the other 2 LEDs maybe you can see the brightness of the remaining LED for each sampled value.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • anhtien
    0 anhtien over 13 years ago

    Jacob,

    1. The code looks better thanks, questions on the current code:

    a. why do you call analogRead twice? I thought you need at least 1ms between reads to get good value.

    b. why do you need to use map etc, you could just do analogWrite(ledx, 0) directly for action a.

    2. The reason for delay of 500ms being too fast: in real life temperature can not change that fast or we are facing end of the world. Let's say you are in a house with this robot you are building and he (or she) has a job of detecting fire.  If there is no fire: green led (or no led on), getting hot: yellow led, red is for the robot being burned.  I believe the right temperature sampling rate would be once every 5 seconds.  Question for you: What do you see on the Serial Monitor screen?  If values change erratically then your sampling is not steady (or something is wrong with the connection).  That would be in conflict with my #3 below.

    3. Assuming you got the sampling steady, there are probably two approaches:

    a.  Each LED goes bright or not (on or off), which is probably what you should start with to make sure your ranges are in good use.

    b.  Getting brighter or dimmer: reading the example "Fade" from Arduino, there is some sort of gradual increase or decrease in value.  Looking at code action c, let's say the sensor reports in the middle range (200 < val < 225), what happen if you have a serie of 200, 210, 202, 225, 215 ?  This is the non-steady situation that the temperature sensor (or pot) might provide, and these values will be spread out (through map function) to 0-255 range.  I believe the LED won't be able to go brighter or dimmer but rather jerking uncontrollably.

    4. Lastly, you might want to try with one LED to see the brightness changes.  Actions b,c,d are for different brightness on 3 LEDS does not seem right, at least looking at the code anyway, try to turn off the other 2 LEDs maybe you can see the brightness of the remaining LED for each sampled value.