Arduino
  • Products
  • More
Arduino
Arduino Forum Attempting to use Switch and Case to Serial.print Date and Time only every 15 minutes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 418 subscribers
  • Views 1306 views
  • Users 0 members are here
  • errors
  • ds1307
Related

Attempting to use Switch and Case to Serial.print Date and Time only every 15 minutes

e14 Contributor
e14 Contributor over 13 years ago

Hello, I am just starting to  work with the Ardunio Uno Rev 3 hardware and re-learning programing; programing experience is from TI 99/4A Extend Basic days!

 

I am working with the Arduio Uno example sketch from the RTCLib, DS1307.

 

Here is what I have so far:

 

//Arduino 1.0+ Only
//Arduino 1.0+ Only

//  Modified DDT DS1307 RTC.ino

#include "Wire.h"
#define DS1307_ADDRESS 0x68
byte zero = 0x00; //workaround for issue #527

void setup(){
  Wire.begin();
  Serial.begin(9600);
  setDateTime(); //MUST CONFIGURE IN FUNCTION
}

void loop(){
  switch(Minute);
  printDate();
  delay(1000);
}

void setDateTime(){

  byte second =      00; //0-59
  byte minute =    13; //0-59
  byte hour =    8; //0-23
  byte weekDay =     6; //1-7
  byte monthDay =    07; //1-31
  byte month =       12; //1-12
  byte year  =       12; //0-99

  Wire.beginTransmission(DS1307_ADDRESS);
  Wire.write(zero); //stop Oscillator

  Wire.write(decToBcd(second));
  Wire.write(decToBcd(minute));
  Wire.write(decToBcd(hour));
  Wire.write(decToBcd(weekDay));
  Wire.write(decToBcd(monthDay));
  Wire.write(decToBcd(month));
  Wire.write(decToBcd(year));

  Wire.write(zero); //start

  Wire.endTransmission();

}

byte decToBcd(byte val){
// Convert normal decimal numbers to binary coded decimal
  return ( (val/10*16) + (val%10) );
}

byte bcdToDec(byte val)  {
// Convert binary coded decimal to normal decimal numbers
  return ( (val/16*10) + (val%16) );
}

void printDate(){

  // Reset the register pointer
  Wire.beginTransmission(DS1307_ADDRESS);
  Wire.write(zero);
  Wire.endTransmission();

  Wire.requestFrom(DS1307_ADDRESS, 7);

  int second = bcdToDec(Wire.read());
  int minute = bcdToDec(Wire.read());
  int hour = bcdToDec(Wire.read() & 0b111111); //24 hour time
  int weekDay = bcdToDec(Wire.read()); //0-6 -> sunday - Saturday
  int monthDay = bcdToDec(Wire.read());
  int month = bcdToDec(Wire.read());
  int year = bcdToDec(Wire.read());
 
 
  
  //print the date EG   3/1/11 23:59:59
  Serial.print(month);
  Serial.print("/");
  Serial.print(monthDay);
  Serial.print("/");
  Serial.print(year);
  Serial.print(" ");
  Serial.print(hour);
  Serial.print(":");
  Switch(minute);
  Serial.print(":");
  Serial.println(second);

}

void Switch(minute){    //  Print only every 15 minutes EG 3/1/11 23:00:00, 23:15:00, 23:30:00, 23:45:00
   
Case 1;
   if (minute) = 00;
   Serial.print(minute);
   break;
Case 2;
   if (minute) = 15;
   Serial.print(minute);
   break;
   Serial.print(minute);
Case 3;
   if (minute) = 30;
   Serial.print(minute);
   break;
Case 4;
   if (minute) = 45;
   Serial.print(minute)
   break;
Default;
   break;
   }

 

 

Verifing the sketch; I have the following errors:

 

sketch_dec08a:15: error: variable or field 'Switch' declared void

sketch_dec08a:15: error: 'minute' was not declared in this scope

sketch_dec08a.ino: In function 'void loop()':

sketch_dec08a:17: error: 'Minute' was not declared in this scope

sketch_dec08a.ino: In function 'void printDate()':

sketch_dec08a:87: error: 'Switch' was not declared in this scope

sketch_dec08a.ino: At global scope:

sketch_dec08a:93: error: variable or field 'Switch' declared void

sketch_dec08a:93: error: 'minute' was not declared in this scope

 

Please, could someone help  to debug this sketch?

 

Thank you.

  • Sign in to reply
  • Cancel
Parents
  • billabott
    0 billabott over 13 years ago

    minute is being used as a global variable and they must be declared before calling the setup() function.

     

    int minute;

     

    and not reused as a locally defined var.

     

       int minute = bcdToDec(Wire.read());

    must change to

       minute = bcdToDec(Wire.read());

     

        int minute = bcdToDec(Wire.read());

    must change to

        minute = bcdToDec(Wire.read());

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago

    minute is being used as a global variable and they must be declared before calling the setup() function.

     

    int minute;

     

    and not reused as a locally defined var.

     

       int minute = bcdToDec(Wire.read());

    must change to

       minute = bcdToDec(Wire.read());

     

        int minute = bcdToDec(Wire.read());

    must change to

        minute = bcdToDec(Wire.read());