Arduino
  • Products
  • More
Arduino
Arduino Forum gps logger 10hz
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 819 views
  • Users 0 members are here
Related

gps logger 10hz

e14 Contributor
e14 Contributor over 13 years ago

Hi my name is Leonardo and I`m new in this and I was wondering if anyone can help me with a little problem I have with my gps logger.

 

I`m using a venus gps, an arduino uno rev3, a mpu6050 and a sd shield. The gps logs perfectly when it is set to 1hz but when puting it at 10hz, strange simbols appears inthe gps data lines in the file logged.

It is not allways and it is only in the gps data part, the mpu6050 is ok.

 

Does anyone knows why this could be?

 

The file is attached, notice that only the gps part has those strange characters

Attachments:
LOGGER00.CSV.zip
  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 13 years ago

    This is just a guess, so I may be wrong:

    I'm not knowledgeable with arduino (or GPS), but it may be worth checking the baud rate. If it is set very low (e.g. 4800bps), then this may be

    insufficient for 10Hz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nabhi
    0 nabhi over 13 years ago in reply to shabaz

    It is the problem with the baud rate. You see the total record length. Calculate the number of bits in a full record. See what is the baud rate set. Calculate whether 10Hz is ok or not You should be able to read the full record in 100ms. If u try to update faster than the read of port, then the garbage comes in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • nabhi
    0 nabhi over 13 years ago in reply to shabaz

    It is the problem with the baud rate. You see the total record length. Calculate the number of bits in a full record. See what is the baud rate set. Calculate whether 10Hz is ok or not You should be able to read the full record in 100ms. If u try to update faster than the read of port, then the garbage comes in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer