Arduino
  • Products
  • More
Arduino
Arduino Forum gps logger 10hz
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 820 views
  • Users 0 members are here
Related

gps logger 10hz

e14 Contributor
e14 Contributor over 13 years ago

Hi my name is Leonardo and I`m new in this and I was wondering if anyone can help me with a little problem I have with my gps logger.

 

I`m using a venus gps, an arduino uno rev3, a mpu6050 and a sd shield. The gps logs perfectly when it is set to 1hz but when puting it at 10hz, strange simbols appears inthe gps data lines in the file logged.

It is not allways and it is only in the gps data part, the mpu6050 is ok.

 

Does anyone knows why this could be?

 

The file is attached, notice that only the gps part has those strange characters

Attachments:
LOGGER00.CSV.zip
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    By full record you mean the amount of bits in 1 second or the amount of bits in one line of data?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    I think you can guesstimate, e.g. assuming that the GPS string is (say) 60 characters long, (and there are 8 bits per character) then that consumes 60*8 = 480bits. Now ten of those per second gets you to 4800 bits-per-sec, and this means that it is highly likely that you do need a higher bitrate than 4800, because the 60 was a guess (it may be 70 or more).

     

    However, I still don't know if that is the cause, it is just a hunch. What is the current baud setting? Is it 4800, 9600 or higher?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    I think you can guesstimate, e.g. assuming that the GPS string is (say) 60 characters long, (and there are 8 bits per character) then that consumes 60*8 = 480bits. Now ten of those per second gets you to 4800 bits-per-sec, and this means that it is highly likely that you do need a higher bitrate than 4800, because the 60 was a guess (it may be 70 or more).

     

    However, I still don't know if that is the cause, it is just a hunch. What is the current baud setting? Is it 4800, 9600 or higher?