Arduino
  • Products
  • More
Arduino
Arduino Forum gps logger 10hz
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 821 views
  • Users 0 members are here
Related

gps logger 10hz

e14 Contributor
e14 Contributor over 13 years ago

Hi my name is Leonardo and I`m new in this and I was wondering if anyone can help me with a little problem I have with my gps logger.

 

I`m using a venus gps, an arduino uno rev3, a mpu6050 and a sd shield. The gps logs perfectly when it is set to 1hz but when puting it at 10hz, strange simbols appears inthe gps data lines in the file logged.

It is not allways and it is only in the gps data part, the mpu6050 is ok.

 

Does anyone knows why this could be?

 

The file is attached, notice that only the gps part has those strange characters

Attachments:
LOGGER00.CSV.zip
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    the baudrate is set to 38400 that is the baudrate for 10hz for the venus gps, so the serial.begin for the sketch is also in 38400, I have tryed with 115200 for the serial.begin for the sketch and its the same result.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    The fact that it is higher than 4800 baud rules out this theory.

    38400 should be more than sufficient.

    It could be that the microcontroller is running with a non-crystal (i.e. non-accurate) oscillator, and maybe the problem was still there at 1Hz, but

    occurred less frequently, since most of your .csv file seems to contain correct data, with few rows containing incorrect

    data.

    At 1Hz, were you using 38400 baud too, or a lower value?

    You probably need to post an image or link to the arduino microcontroller board that you're using.

    Also, I don't know the implementation of the UART API in arduino; maybe you're overrunning a buffer due to the higher bitrate.

    Unfortunately, someone more experienced in Arduino may need to respond to you to help find the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    The fact that it is higher than 4800 baud rules out this theory.

    38400 should be more than sufficient.

    It could be that the microcontroller is running with a non-crystal (i.e. non-accurate) oscillator, and maybe the problem was still there at 1Hz, but

    occurred less frequently, since most of your .csv file seems to contain correct data, with few rows containing incorrect

    data.

    At 1Hz, were you using 38400 baud too, or a lower value?

    You probably need to post an image or link to the arduino microcontroller board that you're using.

    Also, I don't know the implementation of the UART API in arduino; maybe you're overrunning a buffer due to the higher bitrate.

    Unfortunately, someone more experienced in Arduino may need to respond to you to help find the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer