Arduino Forum Self-Destructing arduino code
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
  • State Suggested Answer
  • Replies 29 replies
  • Answers 1 answer
  • Subscribers 406 subscribers
  • Views 3526 views
  • Users 0 members are here
  • self.destructing.arduino.code
Related

Self-Destructing arduino code

dirtdiver
dirtdiver over 12 years ago

Hi everyone,

   so I've been wondering if there is a way to make a hidden button on a device (device wokring with ardunino) that will (once pressed) render the code useless - for example to delete values (val1, val2 ...) or in any way destroy the program that runs that device.

Any ideas?

Thanks,

Lubo (Bo)

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 12 years ago in reply to dirtdiver +2
    Don't patent it! I tell you, it's a waste of time, money and effort. You need to pay thousands of dollars, and here's the worst part: you have to publish a detailed description of your product and how…
  • sonuame
    sonuame over 12 years ago in reply to Former Member +2
    @Rahul,, yeah i am agreed to you , I just told that Reset pin is too much a easy way to stop execution of the microcontroller for that complex machine. sure continously reading the EEPROM values sometimes…
  • ntewinkel
    ntewinkel over 12 years ago in reply to sonuame +2
    I really like Sunil's idea of it only checking after a few days! Much less obvious that way. You might also make it use a jumper on pins instead of a button, to prevent accidental presses. You could probably…
  • sonuame
    0 sonuame over 12 years ago

    Try connecting one I2C EEPROM 24C256, and write the Encrypted string or Code via arduino board. Lets say 1710 is the code you have written in it.

    Now, Atmega328 microcontroler has one onboard EEPROM, Write a code 1710 in it too...

     

    Now in the Setup Section of your code, Compare any I2C device attached to the uC. and make a female socket for the connection of external EEPROM.

     

    Run your whole program of arduino if and only if the internal EEPROM contains 1710 and dont execute if this code is not saved. Once yopu plug in the EXTERNAL EEPROM, define a logic like, if the code of External and Internal EEPROM matches..it will erase the internal EEPROM completly and hence your entire Arduino

    sketch will be useless. Doesnt matter even if you reset it or Power off...

     

    Hope this one helps...!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to sonuame

    Here's an idea:

     

    when the button is pressed, you could just write all the values to 0 (or anything else, if you're trying to confuse the user by giving bogus readings), and put the chip in a never ending loop by using something like this:

     

    while(1)

    {

         //do nothing here, or maybe keep clearing the values if you want

    }

     

    However, the code would start working again when you reset it, or of you power it off and then on again.

     

    What is this mysterious feature for anyway?

     

    One option I can think of (easy way out, no code) is to use a simple SPDT switch to connect the reset pin to ground (that way the micro can't do anything until you open the switch again), but this might not be suited to your (let's be honest, slightly dubious image) purposes. If the switch is hidden well enough, then whoever it's hidden from might not have a clue as to what's going on, unless they're familiar with microcontrollers and have really sharp eyes.

     

    Using the EEPROM to store variables seems a little overkill to me, unless for some reason you want them to be kept after you turn off the chip.

     

    If you want a way to permanently destroy all the code on the chip until it's reprogrammed, it get's a little more complex...

    If you're competent in programming in assembly, maybe you could somehow load the code into the RAM and go from there. This way, the code will vanish once the chip is powered off or reset. This seems like a daunting task to me, and forget using the Arduino environment to do this!

     

    Or you could just set fire to the thing, whatever works best image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 12 years ago in reply to Former Member

    image  image interesting ideas . Anyway i need it becouse im making a racing simulator (http://www.youtube.com/watch?v=y9m--orp8O8)  and the  idea is to put it in a gaming club (i've talked to the owner and its all good), now i know the guy , but its never bad to have a "dead man's switch" in case he decides to pull any stunts i can just "render the sim uselses" and gain leverage image (im also putting a non-resetable timer in it to keep track at the time it was working)

    In other words im just trying to cover all the angles here

    it uses a teensy 3.0 (arduino doesnt have a joystick function) but its programed in the arduino IDE

    i like the idea with the reset pit or a switch keeping the values at 0...i will keep thinking and see whats the best option (maybe all of them)

    I was wondering if there is a way to irreversibly change a value to 0 or something similar so that once pressed the button ruins the code and it has to be reuploaded to the teensy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sonuame
    0 sonuame over 12 years ago in reply to dirtdiver

    Dude,, as per the video attached, I am pretty sure you're gonna mess with lots of Digital circuits and components..then why not a cheap eeprom.

    I am not agreed with the method stated by Mr Rahul. Its not 100% control over your sketch. Protection means real digital protection. Not with any analog means...

     

    4 digit security lock can be easily made just with one keypad and without any microcontroller in it, just by Analog means but its not secure and thats why we use Microcontrollers

    to provide it better security by digital Logics.

     

    Yeah Sure Reset Pin can workout for you but its really not practical.

     

    Make your whole sketch dependant on the values saved on onboard eeprom. And then dedicate a Key somewhere hidden if you want to or you can attach a small keypad if you want, to

    destroy it with some specific code.

     

    When you'll enter exact Code by keypad or you pressed that dead man switch, It should erase the eeprom completly which will make your sketch null and void and won't work until unless you reupload it again.

     

    As per my experience,, This is the Best (I wont say easy)  protection to yor sim...

    and it will be always there even if the power is out

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 12 years ago in reply to sonuame

    i guess you are right, im still gonna have to look into the eeprom couse im not really familiar with it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 12 years ago in reply to dirtdiver

    How about just writing a variable to the built in EEPROM memory?

    http://www.arduino.cc/en/Reference/EEPROM

     

    And then in the loop just check to see if that value is set, and go to the never-ending loop at that point.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 12 years ago

    This is an interesting idea and project. Keep it going and keep us all posted.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago

    Yeah, you have 1K of internal EEPROM to mess around with, and it's dead easy to control with Arduino. You can do what Nico suggested and make the thing check for the important variable first before executing the never ending loop. Something like this (pseudocode, ceebs to write the real thing):

     

    //burn this program to the Arduino first

     

    void setup()

    {

         //write, say, the number 123 to eeprom adress 7 (completely arbitrary numbers I chose)

    }

     

    void loop()

    {

         //nothing to do here

    }

     

    //then erase that old program and write this new one

     

    void setup()

    {

         //whatever your normal code would require in the setup goes here

    }

     

    void loop()

    {

         while(eeprom adress 7 == 123)

         {

              //work properly

     

              if(secret button pressed)

              {

                   //clear EEPROM address 7

              }

     

         }

            lcd.print ("don't mess with a programmer");

    }

     

    I just thought of this code off the top of my head, I'm sure you can make it more efficient, maybe by using interrupts or something. No need for a keypad system or anything, unless you really want some password feature built into it. To reprogram the chip just pull it out of the DIP socket and stick it in your Arduino board, or include an ISP header in your design.

     

    Really cool project btw, hope it all goes well image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 12 years ago in reply to Former Member

    From what I understand, eeprom gets cleared when you upload a new sketch (you might want to test that just to make sure, of course).

     

    Also, from the docs for Read, it mentions that the value will be 255 if that location hasn't been written.

     

    So you'd simply have to do something like this:

     

    void setup() {

    }

     

    void loop() {

     

         while (EEPROM.read(0) == 42) {  // you can use your own favourite number as the flag, of course.

              // self destruct button has been pressed

              // maybe blink a light indicating "malfuntion" ?

         }

     

         // do regular work

     

         if (selfDestructButtonWasPressed()) {

              EEPROM.write(0, 42);

         }

     

    }

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to ntewinkel

    Nico

    The EEPROM doesn't get overwritten with a new sketch.

    You need to clear it. there is an example under the EEPROM library.

     

    There are are limited number of writes, but unlimited reads.

     

    I've been using it to store the date when the Go button is pressed. Each reboot checks to see if the new date is greater then the EEPROM, and acts accordingly.

     

    dirtdiver

    A word of caution.

    I would check to see if 'time bombs' and the like are legal.

    It might pay to ensure the client is aware of these and accepts them. (in writing)

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>