Arduino
  • Products
  • More
Arduino
Arduino Forum Serial communication with arduino using C++
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 503 views
  • Users 0 members are here
  • serial
  • c++
  • arduino
Related

Serial communication with arduino using C++

e14 Contributor
e14 Contributor over 13 years ago

Hi guys,

 

I've been trying to develop some code on C++ using Visual C++ 2008 Express Edition. Inside the code i wanted to use the serial interface to send messages to Arduino, but for some reason it is not working.

When i send messages to the serial port, the Arduino's leds for serial communication don't even blink. I suppose it is not receiving any information, because it doesn't react to incoming messages.

On the C++ side, it creates the serial port succesfully without errors. It also sends message through the serial port without returning any error. What is wrong?

 

In my C++ code I use three different functions: one to initialize serial port, another to close serial port and one to send messages.

 

The code for serial initializing is the following:

 

int initSerial(){

 

hSerial = CreateFile(TEXT("COM11"),                      

                   GENERIC_READ|GENERIC_WRITE, 

                   0,         

                   NULL,                                      

                   OPEN_EXISTING,          

                   0,                                              

                   NULL                                        

                   );

 

 

if(hSerial == INVALID_HANDLE_VALUE)

{

           return false;

}

 

     DCB dcb;

 

if( !GetCommState(hSerial, &dcb))

    return false;

 

dcb.BaudRate = CBR_9600;

dcb.ByteSize = 8;

dcb.Parity = NOPARITY;

dcb.StopBits = ONESTOPBIT;

 

     if( SetCommState(hSerial, &dcb) == 0 )

           return false;

 

}

 

The code for serial closing is the following:

 

void terminateSerial()

{

     CloseHandle( hSerial );

}

 

The code for sending messages to the serial port is:

 

void escreveSerial(char MSG[1000])

{

     DWORD BytesEscritos = 0;

     if(!WriteFile( hSerial, MSG, strlen(MSG), &BytesEscritos, NULL ))

     printf("Error Writefile!\n");

}

 

Has anyone here ever worked with serial communication that could help me?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I found out the problem...

    Apparently, i can only use USB ports named COM1, COM2, ... until COM9.

    As my port was COM11 there was having a problem with the communication.

    '

    I solved this exchanging "COM11" for "\\\\.\\COM11".

     

    Now it works =D

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I found out the problem...

    Apparently, i can only use USB ports named COM1, COM2, ... until COM9.

    As my port was COM11 there was having a problem with the communication.

    '

    I solved this exchanging "COM11" for "\\\\.\\COM11".

     

    Now it works =D

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer