Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Obstacle Avoidance and Cliff Avoidance Robot
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 418 subscribers
  • Views 1676 views
  • Users 0 members are here
  • environment
  • robot
  • development
  • programing
  • arduino
Related

Arduino Obstacle Avoidance and Cliff Avoidance Robot

e14 Contributor
e14 Contributor over 13 years ago

Hello everyone in the Arduino community. Im asking for some help with programing a 3 wheel robot with 2 ultrasonic sensors. The 1st ultrasonic sensor (Parallax)  is used as an obstacle avoidance sensor. The second ultrasonic sensor (SR04) is used to check the ground distance so the robot won't fall into a hole in the ground. The problem I'm having is that the Center Distance Reading from the ultrasonic sensor is always reading zero (0) even if there's nothing in front of the ultrasonic sensors. I have used both of these ultrasonic sensors in another project and they both work perfectly so I now there's nothing wrong with the ultrasonic sensors. I will attach the code I'm using for this project. Thank you in advance for your help.

 

#include <AFMotor.h> // Enables the Motor library

#include <Servo.h> // Enables the Servo library

 

 

Servo PingServo;

AF_DCMotor motor1(1); // Motor 1 is connected to the port 1 on the motor shield

AF_DCMotor motor2(2); // Motor 2 is connected to the port 2 on the motor shield

int minSafeObstacleDist = 11 ; // Minimum distance for ping sensor to know when to turn

int pingPin = A0; // Parallax Ping sensor is connected to port A5

int minSafeGroundDist = 2 ; // Minimum distance for ping sensor to know when to turn

int TrigPin = A5; // SR04 Ping sensor TrigPin is connected to port A5

int EchoPin = A4; // SR04 Ping sensor EchoPin is connected to port A4

int centerDist, leftDist, rightDist, backDist; // Define variables center, left, right and back distance

long duration, inches, cm; // Define variables for Ping sensor

 

void setup() {

PingServo.attach(10); // Servo is attached to pin 10 in the motor shield

PingServo.write(90); // Center the Ping sensor (puts it at 90 degrees)

motor1.setSpeed(250); // Sets the speed of the first motor.

motor2.setSpeed(250); // Sets the speed of the second motor.

 

Serial.begin(9600); // Enables Serial monitor for debugging purposes

Serial.println("Serial test!"); // Test the Serial communication

 

}

 

void AllStop() {

motor1.run(RELEASE); // Turns off motor 1

motor2.run(RELEASE); // Turns off motor 2

}

void AllForward() { // Makes the robot go forward

motor1.run(FORWARD); // Motor 1 goes forward

motor2.run(FORWARD); // Motor 2 goes forward

Serial.println("Going forward"); // Prints a line in the serial monitor

}

void turnRight() { // Makes the robot go right

motor2.run(BACKWARD); // Turns off motor 2

motor1.run(FORWARD); // Motor 1 goes forward

delay(1600); // Time required to turn right (1.6 seconds)

Serial.println("Motors going Right"); // Prints a line in the serial monitor

}

void GoBack(){ // Makes the robot go back

motor2.run(BACKWARD); // Motor 2 goes back

motor1.run(BACKWARD); // Motor 1 goes back

delay(1600); // Time Required to go back (1.6 seconds)

Serial.println("Backward"); // Prints a line in the serial monitor

}

void turnLeft() { // Makes the robot go Left

motor2.run(FORWARD); // Motor 2 goes forward

motor1.run(BACKWARD); // turns off motor 1

delay(1600); //Time Required to turn left (1.6)Seconds

Serial.println("Motors going Left");// Prints a line in the serial monitor

}

// Starts the loop to decide what to do

void loop()

{

LookAhead();

Serial.print(inches);

Serial.println(" inches"); // Prints a line in the serial monitor

if((inches >= minSafeObstacleDist) && (inches <= minSafeGroundDist))/* If the inches in front of an object is greater than or equal to the minimum safe distance A (11 inches) and

floor distance is less than or equal to the minimum safe distance B, react*/

{

AllForward(); // All wheels forward

delay(110); // Wait 0.11 seconds

}else // If not:

 

{

AllStop(); // Stop all motors

LookAround(); // Check your surroundings for best route

if(rightDist > leftDist) // If the right distance is greater than the left distance , turn right

{

turnRight();

}else if (leftDist > rightDist) // If the left distance is greater than the right distance , turn left

{

turnLeft();

}else if (leftDist&&rightDist<minSafeObstacleDist) // If the left and right distance is smaller than the min safe distance (11 inch) go back

{

GoBack();

}

}

}

 

unsigned long ping() {

pinMode(pingPin, OUTPUT); // Make the Pingpin to output

digitalWrite(pingPin, LOW); //Send a low pulse

delayMicroseconds(2); // wait for two microseconds

digitalWrite(pingPin, HIGH); // Send a high pulse

delayMicroseconds(5); // wait for 5 micro seconds

digitalWrite(pingPin, LOW); // send a low pulse

pinMode(pingPin,INPUT); // switch the Pingpin to input

duration = pulseIn(pingPin, HIGH); //listen for echo

unsigned long ping();

pinMode(TrigPin, OUTPUT); // Make the Pingpin to output

digitalWrite(TrigPin, LOW); //Send a low pulse

delayMicroseconds(2); // wait for two microseconds

digitalWrite(TrigPin, HIGH); // Send a high pulse

delayMicroseconds(5); // wait for 5 micro seconds

digitalWrite(TrigPin, LOW); // send a low pulse

pinMode(EchoPin,INPUT); // switch the Pingpin to input

duration = pulseIn(EchoPin, HIGH); //listen for echo

 

/*Convert micro seconds to Inches

-------------------------------------*/

 

inches = microsecondsToInches(duration);

cm = microsecondsToCentimeters(duration);

}

 

long microsecondsToInches(long microseconds) // converts time to a distance

{

return microseconds / 74 / 2;

}

long microsecondsToCentimeters(long microseconds) // converts time to a distance

{

return microseconds / 29 / 2;

}

 

void LookAhead() {

PingServo.write(90);// angle to look forward

delay(175); // wait 0.175 seconds

ping();

}

 

void LookAround(){

PingServo.write(180); // 180° angle

delay(320); // wait 0.32 seconds

ping();

rightDist = inches; //get the right distance

PingServo.write(0); // look to the other side

delay(620); // wait 0.62 seconds

ping();

leftDist = inches; // get the left distance

PingServo.write(90); // 90° angle

delay(275); // wait 0.275 seconds

 

// Prints a line in the serial monitor

Serial.print("RightDist: ");

Serial.println(rightDist);

Serial.print("LeftDist: ");

Serial.println(leftDist);

Serial.print("CenterDist: ");

Serial.println(centerDist);

}

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    This is a really cool idea! I've always wanted to create one of these but have never really had the time or resources. Keep the community posted on your progress!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Yes I will. Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Yes I will. Thank you.