Arduino
  • Products
  • More
Arduino
Arduino Forum arduino drums
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 419 subscribers
  • Views 736 views
  • Users 0 members are here
  • help
  • drums
  • teensy
  • arduino
Related

arduino drums

dirtdiver
dirtdiver over 13 years ago

Hi,

i have been making drums for use with the pc (using Teensy 3.0) but im having trouble with the code - when i trigger the pieso it writes the letter 10-15 times




int ledPin = 13;


byte val = 0;

int statePin = LOW;

int THRESHOLD = 50; // if it's too sensitive then change this value


void setup()

{

pinMode(ledPin, OUTPUT);

}


void loop()

{

val = analogRead(A0);

if (val >= THRESHOLD) { // check the piezo

Keyboard.println("A");

}

delay (10 );



}


I am guessing i have to limit the time in which it reads that "val" is above the THRESHOLD , or maybe somehow implement the fallingEdge function.

Any ideas are highly appreciated!! Thanks

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 13 years ago

    Interesting problem.

    Possibly a delay inside your if-check would help, maybe extended to something like this (pseudo-code):

     

    if (val >= THRESHOLD)

    { // check the piezo

        Keyboard.println("A");

        do

        {

            delay_msec(10);

        } while (val >= THRESHOLD);

    }

     

    The delay outside may still needed as well, as good practice (in case some other process is trying to use the CPU too -

    really depends on the delay implementation - not sure with Arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago

    http://www.arduino.cc/en/Tutorial/KnockSensor may help you understand a little better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    This is an awesome project! Really cool!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 13 years ago in reply to billabott

    That where I startet from, but that code works as a switch, not a button, tap the piezo - turn LED on, tap again- turn off, i need to tap the piezo - light the LED for the duration of the "taping" and the the LED turn off (not actual LED but the teensy's keyboard emulation to press a keyboard key)

     

    My problem right now is that i cantfigure out how to limit the time in which the code reads the >threshold and sends the key press, i tap the piezo and it sends 10-15 times the letter "A" for example and not once.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to dirtdiver

    dirtdiver

    I would suggest when it reaches the threshold, you set a 'flag'.

    Keep reading, and when it falls below the threshold (minus a small amount) you reset the 'flag'

     

    void loop()

    {

    val = analogRead(A0);


    if (val >= THRESHOLD && flag == false) flag = true;

     

     

    if (val <= (THRESHOLD - 2) && flag == true) flag = false;

     

    if(flag == true)    //yes you don't need the ==true

    {

       Keyboard.println("A");

    }

     

    This would send 'A' and as long as it was above threshold (-2) it will keep sending

     

    You can change it to send only once as soon as its above threshold.

    When it drops below threshold -2, it will reset the flag and wait for the next 'hit'.

     

     

    void loop()

    {

    val = analogRead(A0);


    if (val >= THRESHOLD && flag == false)

    {

       Keyboard.println("A");

       flag = true;

    }

     

    if (val <= (THRESHOLD - 2) && flag == true) flag = false;

     

     

    Hope this helps

    mark