Arduino
  • Products
  • More
Arduino
Arduino Forum Serial monitor behaves differently on Windows vs Mac
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 1537 views
  • Users 0 members are here
Related

Serial monitor behaves differently on Windows vs Mac

kjhart0133
kjhart0133 over 13 years ago

A sketch I wrote recently uses Serial.write to display the value read from a potentiometer.  This sketch worked fine on my Mac and displayed correct values on the serial monitor.  When I loaded the exact same sketch onto a Windows platform, instead of displaying the numerical value from the pot, I got ASCII characters.

 

I have limited access to the Windows machine (I'm teaching a group of fifth graders how to use the Arduino) and haven't been able to spend a lot of time debugging this issue.  Any hints would be appreciated.

 

Thanks,

 

Kevin H.

  • Sign in to reply
  • Cancel

Top Replies

  • kjhart0133
    kjhart0133 over 13 years ago in reply to ntewinkel +1
    Nico, I loaded up CoolTerm on my Mac and it works fine. Thanks for the pointer. It's much nicer than the default terminal window that comes with the Arduine IDE (Shift-Cmd-M). CoolTerm doesn't disappear…
Parents
  • kjhart0133
    0 kjhart0133 over 13 years ago

    Sorry, I had to drive up to Minneapolis for two days and just returned.  I've posted the code below, but I don't know if that will help.  I'm using the exact same code on the Mac machine as on the Windows, and it compiles fine on both.  I'll also post a screen shot of the Mac Serial Monitor and the Windows Serial Monitor so you can see the difference.   Unfortunately I won't be on the windows machine until Thursday.  Standby for the screen shots.

     

            • Code Listing ******

     

     

    /*

    Potentiometer SKETCH

    Read level between 5V and Gnd as set by a potentiometer

    */

     

    const int sensorPin = 0;   //select input pin for pot level

    const int ledPin = 13;     //select output pin for LED

    int potlevel = 0;        //variable to store value of light level

     

    void setup()

    {

      Serial.begin(9600);      //send and receive at 9600 baud

      pinMode(ledPin, OUTPUT);  //declare the ledPin as an output

    }

     

    void loop() {

      potlevel = analogRead(sensorPin);  //read voltage on the photosensor pin

      potlevel = map(potlevel, 0, 1023, 0, 255);

      digitalWrite(ledPin, HIGH);          //turn LED on

      delay(100);                   //hold LED on

      digitalWrite(ledPin, LOW);

      delay(100);                  //LED is off for same period as it is on

      Serial.write(potlevel);      // write potlevel to serial output as a byte

    }

     

            • End Listing *****

     

    As to 'credit where credit is due,' I usually do use the CA/HA feature, I just haven't been at my computer in the past couple of days.  Once I get a chance to go over and check out the answers, I'll be sure to give credit.

     

    Thanks,

     

    Kevin H.

     

     

     

    >

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kjhart0133
    0 kjhart0133 over 13 years ago in reply to kjhart0133

    Somehow this solved itself.  I went back to using Serial.println() as Billabot suggested and I am getting the correct values displayed on the Serial Monitor.  Obviously a mental lapse on my part.  Hmmm.

     

    I do have another question, however.  I like to use the Serial Monitor for debug and to monitor data in the sketch.  Each time I upload a sketch due to making corrections or whatever, the Serial Monitor goes away.  I then have to type Shift-Cmd-M to restore it.  Is there any way to keep the Serial Monitor screen from going away each time a sketch is uploaded?

     

    Thanks again,

     

    Kevin H.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to kjhart0133

    I cannot find an answer to your question.  So, what to do?   .... mmmm.....  I think I will  ....  tweet someone who can help us.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to kjhart0133

    And I quote from email just received:

     

     

    hello

     

    the next release of the IDE 1.5 has that… we'll be releasing a new beta soon

     

    m

     

    --

    Massimo Banzi

    Co-Founder Arduino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to billabott

    If you are interested in what the alpha/beta testers are going thru on our behalf you may peruse this Arduino Forum discussion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago in reply to billabott

    If you are interested in what the alpha/beta testers are going thru on our behalf you may peruse this Arduino Forum discussion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer