Arduino
  • Products
  • More
Arduino
Arduino Forum Controlling multiple RGB LEDs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 418 subscribers
  • Views 1398 views
  • Users 0 members are here
  • led_design
  • led
  • rgb
  • arduino_code
  • rgb_led
  • arduino
Related

Controlling multiple RGB LEDs

e14 Contributor
e14 Contributor over 13 years ago

I'm working on a project that requires quite a few RGB LEDs. I would like to have two 5x6 grids (total of 30 LEDs per grid).

I need to acces each LED individually. Is there a special IC or a certain software trick I could use to that would help me with this project?
Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • dmaruska
    dmaruska over 13 years ago +1 suggested
    I have not used this with the Arduion, but have used it in may other projects. But the MAX7300 (I2C) or the MAX7301 (SPI), coupled with some ULN2003 if needed and drive 28 more I/O ports. It's called a…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    You can use a MAX7219CNG serial LED driver, it will interface with an Arduino using only 3 I/O pins and only requires 1 resistor to set the LED brightness, it can directly control up to 64 LEDs.
    They are available at most of the elecrionics suppliers but you can get them cheap on ebay.

     

    Peter W.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Would such logic also be applicable for LED moving message signs? I have always wanted to make my own!!!

    Regards

    Andy

    PS. I am not trying to takeover the blog, just possibly add wider interest.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    If you daisy chain the Dout from one driver to the Din of another driver you can drive as many LEDs as you want using only 3 I/O pins on the Arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    If you daisy chain the Dout from one driver to the Din of another driver you can drive as many LEDs as you want using only 3 I/O pins on the Arduino.