Arduino
  • Products
  • More
Arduino
Arduino Forum Controlling two devices independently(ish)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 416 subscribers
  • Views 541 views
  • Users 0 members are here
  • devices
  • independently
  • controlling
  • two
Related

Controlling two devices independently(ish)

e14 Contributor
e14 Contributor over 13 years ago

Hi,

 

I'm looking for a way to control two devices.  One is a light and based of the proximity it goes on or off....I have that part working now.  The other device needs to be turn on when the light turns on the first time, but then needs  run for 10 mins after no matter if the light is on or off.

 

void loop(void){

 

if  dist1  < onMin){

if dist1 >  onMax)) {

   digitalWrite(lightPin1, HIGH);

   digitalWrite(alarmPin2, HIGH);

}

 

if dist1 < onMax )){

  digitalWrite(lightPin1, LOW);

   }

 

  }

 

}

 

 

Thanks

 

 

 

I'm terribly new to this so pardon my clunky coding.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    HI there,

     

    my first advice would be to use a more comprehensive statement in the if-else condition

    e.g if ( x<a || x>b) "|| means OR you can do it with alt-gr+6 on the top of keyboard"

     

    for the 10mn cooldown i suppose you don't want that your program to be broken on sleep time so you can consider

    using the millis() function that'll not break it using another if-else statement.

    here is a link to be more comprehensive http://arduino.cc/en/Reference/millis and you could also take a look

    at the blink without using delay tutorials to see it in action http://arduino.cc/en/Tutorial/BlinkWithoutDelay

     

    On the other devices you can start it by using a variable containing current state of the device that will be change on the first device at the light on

    e.g

    digitalWrite(ledPin1, HIGH); // the first one on

    if(secondLedState == false){    // check if variable of second led has been used

            secondLedState = ~secondLedState;   // change state of second led

            }

     

    then change the variable as second devices has been triggered.

     

    if(secondLedState == true){

           secondLedState = ~secondLedState;

           }

     

    etc.....

     

    Good luck image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I think that will do nicely!!  I will munch this in my brain a little more and see if I can get it to digest it properly.

     

    Thanks!!