Arduino
  • Products
  • More
Arduino
Arduino Forum Help with Arduino and VFD display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 417 subscribers
  • Views 971 views
  • Users 0 members are here
Related

Help with Arduino and VFD display

symon777
symon777 over 13 years ago

I'm new here - be gentle smiley


I've tried a few other forums and got no response, so I'm hoping you guys can help me out.  I got a few of these displays pretty cheaply, and being I2C I thought they should be pretty easy to get working, problem is I'm stuck.  The datasheet for these displays is here - http://symon.id.au/symon/0900766b80f06185.pdf

 

I get that I need to send a device address byte, then a command or memory address byte, and then the data bytes.  I've found some code on github from someone who has used this display before, unfortunately it was with a PIC not an AVR -https://github.com/Djhg2000/OpenHUDisplay/blob/master/m12by02aa.c


The code I am using so far is below, just to try to turn one of the three LED's on, but nothing I seem to do is working.  Any help is greatly appreciated.

 

#include <Wire.h>
byte I2C_add = B10100000; //address #0
byte disp_write = B01000000; //write to display memory
byte disp_bright = B10011111; //turn on display, maximum brightness
byte led_write = B01000101; //write to LED's




void setup() {
  Wire.begin();
}


void loop() {
  Wire.beginTransmission(0); 
  Wire.write(I2C_add); //write to address #0
  Wire.write(disp_bright); //turn on display
  Wire.endTransmission();
  delay(250);
  Wire.beginTransmission(0);
  Wire.write(I2C_add);
  Wire.write(led_write); //write to LED
  Wire.write(B01000101); //turn LED 2 on
  Wire.endTransmission();
  delay(1000);
}

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +2 verified
    i2c address should be used as an argument to beginTransmission function on Arduino, like this: Wire.beginTransmission(I2C_addr); Wire.write(disp_bright); //turn on display Wire.endTransmission();
  • symon777
    symon777 over 13 years ago in reply to e14 Contributor +1
    Of course! It is always the easy things that are hardest to find! Thank you. The other thing I found out is that the standard Arduino Wire() library only uses 7-bit addressing, and adds the extra RW bit…
Parents
  • billabott
    0 billabott over 13 years ago

    Friend, would ye be willing to share source and pricing for this fine wee trinket?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to billabott

    Also a photo of it in action - it looks nice : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • symon777
    0 symon777 over 13 years ago in reply to shabaz

    As requested here are a couple of photos.  I have used the display for a GPS clock.  The LED's on the left side show the GPS sync status - green means the time is in sync with the GPS, and amber means there is no GPS fix and the time is being read from the RTC.  The GPS module I am using is a Skylab SKM53, and the RTC is a DS3232 - which also has a internal temperature sensor so I am displaying that as well.

    Attachments:
    image
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • symon777
    0 symon777 over 13 years ago in reply to shabaz

    As requested here are a couple of photos.  I have used the display for a GPS clock.  The LED's on the left side show the GPS sync status - green means the time is in sync with the GPS, and amber means there is no GPS fix and the time is being read from the RTC.  The GPS module I am using is a Skylab SKM53, and the RTC is a DS3232 - which also has a internal temperature sensor so I am displaying that as well.

    Attachments: