Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino SPI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 416 subscribers
  • Views 448 views
  • Users 0 members are here
Related

Arduino SPI

e14 Contributor
e14 Contributor over 13 years ago

I connected my clock pin to an o-scope and I am not getting any clock signal from it. Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    You have to initialize SPI for it to work, something like this: SPI.begin(); SPI.setDataMode(SPI_MODE0); SPI.setClockDivider(SPI_CLOCK_DIV16); SPI.setBitOrder(MSBFIRST); and then you can use SPI.transfer…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    You have to initialize SPI for it to work, something like this:

    SPI.begin();

    SPI.setDataMode(SPI_MODE0);

    SPI.setClockDivider(SPI_CLOCK_DIV16);

    SPI.setBitOrder(MSBFIRST);

     

    and then you can use SPI.transfer to send/receive data.

    Please refer to http://arduino.cc/en/Reference/SPI and carefully read the section that describes Slave Select pin, if it is configured for input before you call SPI.begin() you can end up operating SPI hardware in slave mode and clock will not be generated then.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    You have to initialize SPI for it to work, something like this:

    SPI.begin();

    SPI.setDataMode(SPI_MODE0);

    SPI.setClockDivider(SPI_CLOCK_DIV16);

    SPI.setBitOrder(MSBFIRST);

     

    and then you can use SPI.transfer to send/receive data.

    Please refer to http://arduino.cc/en/Reference/SPI and carefully read the section that describes Slave Select pin, if it is configured for input before you call SPI.begin() you can end up operating SPI hardware in slave mode and clock will not be generated then.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for the response. I have tried initializing the SPI by writing the exact code minus the SPI.setDataMOde(SPI_MODE0). I will try that and see what happens.