Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Library Compiler Errors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 418 subscribers
  • Views 1655 views
  • Users 0 members are here
  • help
  • .h
  • library
  • library_editor
  • code_libraries
  • .cpp
  • arduino_development_environment
  • error
  • compilier
  • arduino
Related

Arduino Library Compiler Errors

8163jb
8163jb over 13 years ago

Hey, I have recently attempted to make a library which enables users to put a scrolling text command along with their AXE133Y Picaxe OLED display, here is the header code:

 

 

     #ifndef ScrollText_h

     #define ScrollText_h

 

 

     #include "Arduino.h"

     #include <AXE133Y.h>

 

 

     class ScrollText

     {

       public:

         scroll(String input);

         String input;

       private:

         String _input;

         int _blank;

         String _output;

         String _output2;

         int _amount;

         char _charBbuf[];

         int _pos;

         int _poss;

     };

 

 

     #endif

 

And here is the .cpp file:

 

     #include "Arduino.h"

     #include "ScrollText.h"

     #include <AXE133Y.h>

 

 

     AXE133Y OLED = AXE133Y(1);

 

 

 

 

     void ScrollText::scroll(String input)

     {

       String _input = input;

       for (int _blank = 16; _blank > 0; _blank--)

       {

         String _output = "";

         String _output2 = "";

         for(int _amount = _blank; _amount >= 0; _amount--)

         {

           _output = _output + " ";

         }

         for (int _amount = 16 - _blank; _amount >= 0; _amount--)

         {

           _output2 = _output2 + " ";

         }

         _output = _output + _input + _output2;

         OLED.cursorHome(1);

         OLED.print(_output);

         delay(150);

       }

       OLED.cursorHome(1);

       OLED.print(" " + _input + " ");

       OLED.cursorHome(1);

       delay(170);

       char _charBuf[_input.length()];

       _input.toCharArray(_charBuf, _input.length() + 1);

       for (int _pos = 0; _pos <= _input.length(); _pos++)

       {

         OLED.cursorHome(1);

         for(int _poss = _pos; _poss <= _input.length(); _poss++)

         {

           OLED.print(String(_charBuf[_poss]));

         }

         OLED.print(" ");

         delay(150 + (_input.length() / 1.5));

       }

       OLED.clearScreen();

     }

 

I can't find any errors with this, yet when I put this code into the Ardunio IDE:

 

     #include <ScrollText.h>

 

 

     void setup()

     {

       ScrollText.scroll("Hello World");

     }

 

 

     void loop()

     {

     }

 

It returns the following errors:

 

"In file included from sketch_feb06a.ino:1:

C:\file system etc... \arduino\libraries\ScrollText/ScrollText.h:14: error: ISO C++ forbids declaration of 'scroll' with no type

sketch_feb06a.ino: In function 'void setup()':

sketch_feb06a:5: error: expected unqualified-id before '.' token"

 

Can anyone tell me why this is happening and how I can fix it? Cheers in advance!

Tom C (15)

  • Sign in to reply
  • Cancel
Parents
  • weissar
    0 weissar over 13 years ago

    Hi, compiler says - " ISO C++ forbids declaration of 'scroll' with no type", so you must write type in declaration of function scroll:

     

    ...

      public:

             void scroll(String input);

    ...

     

    Petr

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 8163jb
    0 8163jb over 13 years ago in reply to weissar

    I tried what you said and it sorted out that error, so thankyou very much, however, I still get this error when running the code:

     

    sketch_feb06a.ino: In function 'void setup()':

    sketch_feb06a:5: error: expected unqualified-id before '.' token"

     

    Any ideas what I have done wrong here?

     

    Cheers in advance!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to 8163jb

    Did you pull your library from here: https://github.com/ratbum/ScrollText ?

     

    It says it is for 7-Segment display being driven by single shift register.

     

    I don't know, but it might be helpful if we knew where the .h libraries are sourced from.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 8163jb
    0 8163jb over 13 years ago in reply to billabott

    No I wrote it all myself, It is for a 16X2 OLED display. All the code available is in the original post

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to 8163jb

    Tom,

      Try using a double colon "::" which is the scope resolution operator in c++,

    unlike other languages like Java and Ada.

     

        ScrollText::scroll("Hello World");

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 8163jb
    0 8163jb over 13 years ago in reply to e14 Contributor

    Thanks very much, i've tried running this code now:

     

    #include <ScrollText.h>

     

     

    void setup()

    {  

      ScrollText::scroll("Hello World");

    }

     

     

    void loop()

    {

    }

     

    I didn't realise C++ had a different scope resolution operator, oops!

    However, now I get this error instead:

     

    sketch_feb21b.ino: In function 'void setup()':

    sketch_feb21b:5: error: 'scroll' is not a member of 'ScrollText'

     

    But as far as I can tell it should be a member? Any Ideas? Cheers in advance!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to 8163jb

    I am guessing that

     

    AXE133Y OLED = AXE133Y(1);

     

         void ScrollText::scroll(String input)

         {

           String _input = input;

     

    should read:

     

    AXE133Y OLED = AXE133Y(1);

     

        void scroll(String input)

         {

           String _input = input;

     

    OR

     

    that the scroll() function should be completely defined inside the ScrollText.h

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago in reply to 8163jb

    I am guessing that

     

    AXE133Y OLED = AXE133Y(1);

     

         void ScrollText::scroll(String input)

         {

           String _input = input;

     

    should read:

     

    AXE133Y OLED = AXE133Y(1);

     

        void scroll(String input)

         {

           String _input = input;

     

    OR

     

    that the scroll() function should be completely defined inside the ScrollText.h

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • 8163jb
    0 8163jb over 13 years ago in reply to billabott

    Thanks very much but I realised I had a capital for 'scroll' in my header file, which was bringing up all the errors. It now seems to recognise it as a command but when I run this code:

     

    #include <ScrollText.h>

     

     

    void setup()

    {  

      ScrollText::scroll("Hello World");

    }

     

     

    void loop()

    {

    }

     

    it is bringing up the following error:

     

    error: cannot call member function 'void ScrollText::scroll(String)' without objects

     

    cheers in advance! Sorry this is the first library I have attempted to write!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 8163jb
    0 8163jb over 13 years ago in reply to 8163jb

    Sorry, cancel that, I didn't realise I had to define it as an object! So now instead of this code:

     

    #include <ScrollText.h>

     

     

    void setup()

    {  

      ScrollText::scroll("Hello World");

    }

     

     

    void loop()

    {

    }

     

    I'm running this code:

     

    #include <ScrollText.h>

     

    ScrollText ST;

     

    oid setup()

    {  

      ST.scroll("Hello World");

    }

     

     

    void loop()

    {

    }

     

    Thanks very much!