Arduino
  • Products
  • More
Arduino
Arduino Forum how to output 3.3 volts in atmega328p?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 418 subscribers
  • Views 4978 views
  • Users 0 members are here
  • atmega328p
  • 3.3v
Related

how to output 3.3 volts in atmega328p?

rishi2628
rishi2628 over 11 years ago

I want the atmega328p to output 3.3 volts on the pin, when i use the digitalWrite function in arduino.Will it be possible if i use 3.3 volts to power the microcontroller rather than 5 volts. PS in the datasheet it says that the microcontroller operates in the range of 1.8 volts to 5.5 volts.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    An Arduino UNO is designed to work at 5V, you would need to change components to get it to work at 3V3 including the Crystal (Lower Voltage = Lower Speed) two diodes in series or a resistor divider would…
  • mcb1
    mcb1 over 11 years ago +1
    Some boards have a 5v/3v3 switch option. This allows the whole board to work at 3v3 rather than 5v. This may an option. Mark
  • ravi_butani
    ravi_butani over 11 years ago +1
    U can put atmega328 on breadboard and use it with 3.3V supply on VCC and AVCC pins of Atmega328 Better option is If you want to use 3.3V logic on any pin of arduino, just put resistor divider network on…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    An Arduino UNO is designed to work at 5V, you would need to change components to get it to work at 3V3 including the Crystal (Lower Voltage = Lower Speed)

     

    two diodes in series or a resistor divider would work if only used for output.

     

    the other option is a level shifter like this SN74LVC245ADWR - TEXAS INSTRUMENTS - IC, 74LVC, SMD, 74LVC245, SOIC20 | Farnell element14

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    An Arduino UNO is designed to work at 5V, you would need to change components to get it to work at 3V3 including the Crystal (Lower Voltage = Lower Speed)

     

    two diodes in series or a resistor divider would work if only used for output.

     

    the other option is a level shifter like this SN74LVC245ADWR - TEXAS INSTRUMENTS - IC, 74LVC, SMD, 74LVC245, SOIC20 | Farnell element14