Arduino
  • Products
  • More
Arduino
Arduino Forum Bootloader fails with replacement ATMega328 chip in Arduino Uno
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 417 subscribers
  • Views 522 views
  • Users 0 members are here
  • bootloader
  • atmega328
  • uno
Related

Bootloader fails with replacement ATMega328 chip in Arduino Uno

e14 Contributor
e14 Contributor over 13 years ago

I am trying to program a new ATMega328 chip by plugging it into an Arduino Uno board in place of the existing chip of the same type, but I find that, although the replacement chip successfully runs the default test program (ie, it flashes the LED), it  does not responds to downloads from the Arduino Environment.

 

In more detail:

  • The Uno board (Farnell #2075382) is Rev 3.  It faultlessly accepts downloads from the Arduino IDE (running under Windows 7) when it has its original chip in place.
  • The spec for the replacement chip (Farnell #1848694) states that it is preprogrammed with a Uno bootloader.
  • The original chip and the replacement one are both marked ATMega328P-PU (but they do have different numbers tagged on: the original chip has “1230”, the replacment one “1201”).
  • The default program on the original chip flashes the LED about once a second indefinitely; the replacement chip flashes it 4 times at about the same rate, then stops.
  • The Arduino IDE fails to download sketches when the replacement chip is in place. (Specifically, avrdude reports “avrdude: stk500_getsync(): not in sync: resp=0x00”.)

 

It looks as if there may be some incompatibility between the bootloader in the replacement chip and either the Arduino board or the current Arduino IDE.  Does anyone have any suggestions?

  • Sign in to reply
  • Cancel
Parents
  • Hassan.elbaytam
    0 Hassan.elbaytam over 13 years ago

    I got the same problem , but the thing is i removed the oringinal chip and put it back .. now the arduino IDE wont let me upload sketchs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Hassan.elbaytam
    0 Hassan.elbaytam over 13 years ago

    I got the same problem , but the thing is i removed the oringinal chip and put it back .. now the arduino IDE wont let me upload sketchs