Arduino
  • Products
  • More
Arduino
Arduino Forum please help me in selecting the appropriate Arduino board for my project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 416 subscribers
  • Views 433 views
  • Users 0 members are here
Related

please help me in selecting the appropriate Arduino board for my project

e14 Contributor
e14 Contributor over 13 years ago

Hello,

                       I am working on 3 phase induction motor.In this project the voltage and current values from the motor are to be displayed on a PC and corresponding graph has to be displayed.Since I am a beginner to Arduino ,Please help me find a suitable  Aurdino board  with following features.

6 ADC pins

compatible with android(Further I want to display graphs on android device)

SD card facility to store the values.

 

please help me choosing the board with above features in following cases

 

1.connectivity : serial communication.

 

2.wifi communication.

 

3.ethernet communication.

 

If any one has an idea regarding this project ,please help me.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Arduino Ethernet coupled with a wireless SD shield?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The only two boards that are compatible with android devices are the Mega ADK board and the Due is also capable of hosting an android device. On top of those you'll need whatever shield you are wanting to use, i would guess the WiFi shield would be more what you're looking for however. The ADK board costs a bit more, however it'll be more compatible with any shield you want for the board due to the new Due running on a 3.3 V logic instead of 5 V. The Due is more powerful but less cross compatibility. Either should work for your intended purpose. I personally went with the Due, just my $0.02.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Arduino Uno would be the best choice 4 u..