Arduino
  • Products
  • More
Arduino
Arduino Forum A quick question on backup power
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 1000 views
  • Users 0 members are here
  • supply
  • power
  • arduino
Related

A quick question on backup power

dirtdiver
dirtdiver over 13 years ago

Hi everyone,

im making a model house with a solar panel and a rechargable battery.I've been looking on the internet for a while, but i cant really find out if what im planning to do is correct in terms of wiring.

Idealy you will have the external power disconnected and the battery will be charged by the solar panel and drained by the consumers (servo+ a few LEDs) and when the energy is not enought the external power will charge the battery/ or if the power network is down- rely on the solar energy to charge the battery alone.

 

Is this schematic applicable?

 

Im not sure if i have to put any diods around to limit the current's direction

 

**For some reason i cant insert an image so im attaching it as a file!

 

Thans in advance!

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 13 years ago in reply to phoenixcomm +2
    For a small toy house, you shouldn't need a lot. Your cct doesn't give you much voltage headroom to efficently control it. I would tend to try 12v and then use a regulator to drop it down to 5v for your…
  • dirtdiver
    dirtdiver over 13 years ago +2
    The final project http://www.youtube.com/watch?v=gnkAlNlPg_4&feature=youtu.be
  • shabaz
    shabaz over 13 years ago in reply to ntewinkel +1
    Hi Nico, I think you're right, I think some Lead Acid, e.g. possibly burglar alarm batteries, can be charged like this as long as you like. One thing possibly worth doing would be to have a cut-off that…
Parents
  • ntewinkel
    0 ntewinkel over 13 years ago

    I've been looking into this sort of thing a little bit, as I need to do something about the solar setup in my outbuilding (wife's art gallery) now that the charge controller seems to have died.

     

    From what I understand, as long as the maximum charge amps of the solar cell is at a rate small enough compared to the total battery capacity (ie, the equivalent of a trickle charge), you don't actually need any circuitry (other than that diode I guess) - the battery will just dissipate the extra energy in the form of a small amount of warmth.

    But I'm using basic lead-acid batteries in my setup, so that might not apply to your NiCd battery.

     

    I could also be very very wrong, and if so I hope someone will correct me before I blow up my wife's art gallery image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 13 years ago

    I've been looking into this sort of thing a little bit, as I need to do something about the solar setup in my outbuilding (wife's art gallery) now that the charge controller seems to have died.

     

    From what I understand, as long as the maximum charge amps of the solar cell is at a rate small enough compared to the total battery capacity (ie, the equivalent of a trickle charge), you don't actually need any circuitry (other than that diode I guess) - the battery will just dissipate the extra energy in the form of a small amount of warmth.

    But I'm using basic lead-acid batteries in my setup, so that might not apply to your NiCd battery.

     

    I could also be very very wrong, and if so I hope someone will correct me before I blow up my wife's art gallery image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 13 years ago in reply to ntewinkel

    Hi Nico,

     

    I think you're right, I think some Lead Acid, e.g. possibly burglar alarm batteries, can be charged like this as long as you like. One thing possibly worth

    doing would be to have a cut-off that constantly monitors the battery voltage, and cuts off the solar cell (or reduces the charge current)

    if the voltage exceeds approx 13.8-14V (usually marked as the float voltage in the datasheet for the battery) for a 12V battery.

     

    For NiCd, some batteries (usually the larger ones, e.g. 'D') can be indefinitely trickle-charged (i.e. topped up) as long as the current is kept low (e.g. a series resistor), and probably trickle-charging like this doesn't apply to newer rechargeable type chemistries.

    If you wish to charge at a higher rate too (i.e. when the solar cell can supply the power, and when the battery does need more than trickle charging),

    then for both lead-acid and NiCd,  you know when the battery is charged by looking at dV/dT which will rise as a symptom of end-of-charge being reached (easy to monitor this with a dedicated IC I guess). If there are cold conditions, NiCd was preferred over Lead Acid for more efficient charging in the cold, but maybe manufacturers have resolved this nowadays.

     

    In the past some older charger ICs just relied on dV/dT, some on just time, etc., but a combination (including temperature) is good

    for safety, for NiCd and NiMH batteries. Modern ICs support the combination of charge termination conditions (with no charge termination, if the current is too high, even large NiCd batteries will eventually pop (I guess as you say, the heat doesn't reach the steady-state at this high level of energy) and has to go somewhere : ) I saw that occur once, not pretty!

     

    Li-Ion are super-sensitive and possibly best served with specialized charger ICs always.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 13 years ago in reply to shabaz

    Thanks for the advice, Shabaz image

     

    I've decided to just buy a controller for my setup - easiest way to make sure all is well, and it turns out their not that expensive anymore.