Arduino
  • Products
  • More
Arduino
Arduino Forum GPS receiver project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 417 subscribers
  • Views 1831 views
  • Users 0 members are here
Related

GPS receiver project

e14 Contributor
e14 Contributor over 13 years ago

Hello everyone,

 

I am looking to make a GPS receiver for a project. It is part of a project to assist the visually impaired get around easier on campus. The application of the receiver would be to tell the user how far he/she is from a building. I would also like to include audio feedback to let the user know the name of the particular building he/she is close to. I have looked into different GPS modules.   Working with an Arduino board is what I prefer to use with the module. What modules are recommended? Should I make a logger or live tracking? How should I go about including audio feedback? I mainly need some places to start in order to begin. Thanks for the advice in advance.

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    0 mcb1 over 13 years ago

    Have a look at the work these guys did with GPS.

    They built a seperate board that acted as a RTC, SD card and host for the GPS functions.

    http://wyolum.com/shop/20-i2gps.html

     

    Audio is available in multiple different ways from simple tones, to tunes played from ram. Do a Google search.

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    Thanks Mark, I'll look into it more.

     

    I reserved my parts today from MicroCenter. The parts I reserved was a, gps module, micro sd shield, and a arduino mega. All of the parts are Sparkfun. The only part that the store didn't have was a gps shield. I have to order it on another website. How important is the gps shield? Can I work around it to get the receiver to work while I wait for the shield to arrive?

     

    The links to the parts are below.

     

    http://www.microcenter.com/product/389895/66_Channel_LS20031_GPS_10Hz_Receiver

    http://www.microcenter.com/product/392636/Arduino_Mega2560_Rev_3

    http://www.microcenter.com/product/389841/microSD_Shield

    http://www.microcenter.com/product/389881/GPS_Shield

     

    They have a GPS shield that is separate as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to e14 Contributor

    I would think you should be able to get it to work using the MicroSD shield.

    I'm not sure how an Arduino shield translates to the Mega, so you might need to look at cables.

     

    That GPS is expensive. The UP501 that the Wyolum boys use was only NZ$50, and the GPS shield includes the 401 which is why it was expensive.

     

    The i2GPS board is looking better all the time. (FYI I wired the A0-A4 pins out to the normal place with some jumpers to give extra I/O.)

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    The module is pretty expensive. I am thinking of it getting due to time and I need to get it working by the end of next week. I plan on following some tutorials from the element 14 arduino forum to get the gps to work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to e14 Contributor

    Nothing like the added pressure of a deadline.

    Its a fairly serious project that deserves a reasonable amount of solution options to decide on the best method.

     

    If I was undertaking this I think I would be looking at a small SBC (single board computer) or tablet.

    The reason is you still have to map the locations of these buildings and store that somewhere.

    Knowing where you are is only part of the solution.

     

    There is a fair amount of this work already done with the ArduRover guys (http://code.google.com/p/ardurover/ )

    This might be of some help.

     

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    Is there anyway I can translate the code from the ArduRover to an Arduino? I was going to go over the tutorial from Jeremy Blum, http://www.youtube.com/watch?v=TtZEZYQG0xk&list=ECA567CE235D39FA84&index=15. Im following from the parts that he had.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    Is there anyway I can translate the code from the ArduRover to an Arduino? I was going to go over the tutorial from Jeremy Blum, http://www.youtube.com/watch?v=TtZEZYQG0xk&list=ECA567CE235D39FA84&index=15. Im following from the parts that he had.