Arduino
  • Products
  • More
Arduino
Arduino Forum What about Analog Outputs?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 550 views
  • Users 0 members are here
Related

What about Analog Outputs?

billabott
billabott over 13 years ago

It is easily understood that the Arduino family of microcontrollers are able to do digital input and digital output with  digitalRead() and digitalWrite().  And because of the onboard ADC the UNO and others can do analog input using analogRead(). 

 

But, what about the need for analog output?  Like when the LED really needs to gently brighten and dim slowly rather that the harshness of instant full on and instant off.  Atmel certainly could have added a few hundred more transistors to the silicon die and included an onboard DAC.  They did not.

 

Would the UNO be better if they had included the DAC?

  • Sign in to reply
  • Cancel

Top Replies

  • ntewinkel
    ntewinkel over 13 years ago +2
    Hi Billabott, The Arduino does have analogWrite, but I guess they fake it using PWM, and I think the increments might be a bit rough (values range from 0-255). To brighten and dim LEDs you can do that…
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    I could see a few different reasons they didn't want to include it. First would be cost. Always better to keep cost down. Second would be that different DACs are used for different things. An audio DAC…
  • mcb1
    mcb1 over 13 years ago in reply to ntewinkel +1
    Bill I tend to agree that cost would be a factor, but not having a complete understanding of the inner working on the ATmel chip (they make them too small for my eyesight), I'm guessing that in most uP…
Parents
  • ntewinkel
    0 ntewinkel over 13 years ago

    Hi Billabott,

     

    The Arduino does have analogWrite, but I guess they fake it using PWM, and I think the increments might be a bit rough (values range from 0-255).

    To brighten and dim LEDs you can do that using analogWrite, as in the Fading demo that comes with Arduino (Examples-03.Analog-Fading). But it could be more gentle for sure.

     

    I'm not sure what the reasoning is - maybe cost is a factor and PWM is "close enough"?

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 13 years ago

    Hi Billabott,

     

    The Arduino does have analogWrite, but I guess they fake it using PWM, and I think the increments might be a bit rough (values range from 0-255).

    To brighten and dim LEDs you can do that using analogWrite, as in the Fading demo that comes with Arduino (Examples-03.Analog-Fading). But it could be more gentle for sure.

     

    I'm not sure what the reasoning is - maybe cost is a factor and PWM is "close enough"?

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 13 years ago in reply to ntewinkel

    Bill

    I tend to agree that cost would be a factor, but not having a complete understanding of the inner working on the ATmel chip (they make them too small for my eyesight), I'm guessing that in most uP applications PWM is enough.

     

    PWM is not available on all outputs, and there is a very excellent refererence done here, that every Arduino user should download.

    http://arduino.cc/forum/index.php?PHPSESSID=16e64b1ad04ca4b8263c52d65465e238&topic=146315.0

     

    As Nico said there are examples of PWM, and some even include the 'map' feature to convert the 0-1023 of the analogue input to 0-254 of the PWM output.

     

    To answer your question "... Would the UNO be better if they had included the DAC?"

    IMO No because it would be more expensive.

     

    If the design requires it, then there are aftermarket chips to provide a DAC that would do a better job.

     

     

    @Robert

    You can set the Analogue reference voltage using external ( http://arduino.cc/en/Reference/AnalogReference ), so you could do something with a resistor divider from the 5 or 3v3 regulator if you wanted to.

     

    Cheers

    Mark