Arduino
  • Products
  • More
Arduino
Arduino Forum stepper motor with arduino and labview
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 417 subscribers
  • Views 993 views
  • Users 0 members are here
  • arduino
Related

stepper motor with arduino and labview

e14 Contributor
e14 Contributor over 13 years ago

Hi guys,

For a project Im trying to control a stepper motor using labview. Im totally new to motors and electronics and greatly appreciate your help. If I use a NEMA 17 stepper motor and a stepper driver (P70530 by NI) can I use an Adruino micro-controller to control the motor rather than a NI motion controller or a DAQ device (which are pretty expensive) and then interface with labVIEW coding? If so would I be connecting the stepper driver with the Adruino? (i.e: motor-.>stepper driver-->Adruino-->PC-labview coding). As I said I've had no experience with these stuff..so please help !!

Thanks!!!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Guys,

    Can someone tell me if Arduino micro-controllers are compatible with any type of stepper motor drives? And what exactly is a motor shield drive? Do I need that to run the motor? Im clueless about it image  It would be great if someone could list all the stuff I need to run a NEMA 17 type motor using Arduino interfaced by labVIEW.

    Please help !! Thank you so much !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 13 years ago in reply to e14 Contributor

    I think this example from Arduino.cc will help you: http://arduino.cc/en/Tutorial/MotorKnob

     

    It also explains stepper motors a bit - apparently there are two kinds, and it looks like either type will work with Arduino.

     

    A motor drive shield is basically a board you plug into the Arduino that makes it easier to control a motor.

    And from the example it looks like you don't need a shield, but it does look like you need a chip (the kind depends on the kind of stepper motor).

     

    I don't know much about labView, but given that it can be done using the basic Arduino IDE, I would assume that the same thing can be done using other IDEs.

     

    Good luck with the project, I hope this helps.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 13 years ago in reply to e14 Contributor

    I think this example from Arduino.cc will help you: http://arduino.cc/en/Tutorial/MotorKnob

     

    It also explains stepper motors a bit - apparently there are two kinds, and it looks like either type will work with Arduino.

     

    A motor drive shield is basically a board you plug into the Arduino that makes it easier to control a motor.

    And from the example it looks like you don't need a shield, but it does look like you need a chip (the kind depends on the kind of stepper motor).

     

    I don't know much about labView, but given that it can be done using the basic Arduino IDE, I would assume that the same thing can be done using other IDEs.

     

    Good luck with the project, I hope this helps.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to ntewinkel

    Thank you so much for the help Nico !!!