Arduino Forum Issue with Ardumoto and SR04 sensor
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
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 394 subscribers
  • Views 588 views
  • Users 0 members are here
  • robot
  • arduino
Related

Issue with Ardumoto and SR04 sensor

Former Member
Former Member over 12 years ago

I am using the Ardumoto board on a Magician chassis with the HC-SR04 ultrasonic sensor to check for obstacles.

I am using standard code to check for obstacles (using the NewPing.h library). However, though the obstacle checking code and the code to run the motors work fine by themselves, when I use the two in conjunction, the ultrasonic sensor always returns the wrong distance (always about 4 - 5 cm).

 

Here is the code - any help appreciated!

 

#include <NewPing.h>

#define pingPin  8 

#define trigPin  7

#define MAX_DISTANCE 200

 

// pins for motor speed and direction

int speed1 = 3, speed2 = 11, direction1 = 12, direction2 = 13;

int startSpeed = 150;

 

long duration; //time it takes to receive bounced back signal

const int dangerThresh = 15; //threshold for obstacles (in cm)

 

NewPing sonar(trigPin, pingPin, MAX_DISTANCE); // NewPing setup of pin and maximum distance.

 

// initial speeds of left and right motors

int left = startSpeed, right = startSpeed;

 

 

void setup() {

 

  pinMode(trigPin, OUTPUT);

  pinMode(pingPin, INPUT);

  pinMode(9, OUTPUT);  // led

 

// set the motor pins to outputs

  pinMode(speed1, OUTPUT);

  pinMode(speed2, OUTPUT);

  pinMode(direction1, OUTPUT);

  pinMode(direction2, OUTPUT);

 

  delay(1000); 

  // make both motors same speed

  left = startSpeed;

  right = startSpeed;

  Serial.begin(115200);

}

 

void loop() {

 

  // read the sensor

  delay(50);

  int distanceFwd = sonar.ping();

  distanceFwd = distanceFwd/US_ROUNDTRIP_CM;

 

  while ((distanceFwd<dangerThresh) && (distanceFwd!=0)) { //if path is blocked

    Serial.print("dist: ");

    Serial.println(distanceFwd);

    goBeep();

    distanceFwd = sonar.ping();

    distanceFwd = distanceFwd/US_ROUNDTRIP_CM;  

    // no logic yet to stop the motors... just testing...

  }

 

  // no obstacle, so move ahead

  // if I comment out the moveAhead() line below, I get the correct distance,

  // otherwise I always get a distance of about 4 - 5 cm

  moveAhead();}

 

 

// was using a buzzer first to beep when obstacle detected.

// but just have an LED on Pin 9 now...

void goBeep() {

  analogWrite(9, 20);                            

  delay(200);         

  analogWrite(9, 0);      

  delay(200);

}

 

void moveAhead() {

// set motor direction to forward

  digitalWrite(direction1, HIGH);

  digitalWrite(direction2, HIGH);

// set speed of both motors

  analogWrite(speed1,left);

  analogWrite(speed2,right);   

}

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 12 years ago in reply to billabott +1
    I have fixed the problem - thanks to the hint in your first reply! I was using the same power supply for both the ultrasonic sensor and the motors... I have just fixed up another power supply for the sensor…
Parents
  • billabott
    0 billabott over 12 years ago

    Please clarify.  Without changing the sketch, disconnect the pins that control the motor.  Does the ping))) sensor return correct values?

     

    If it does, then you could have a poorly isolated H-bridge that is dumping a surge (spikes) on the ground plane power supply rails. 

     

    There are two Ardumoto - Motor Driver Shields from Sparkfun:   DEV-09815 and DEV-09213

     

    What motors are you using?  Provide a full designation please.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to billabott

    I have fixed the problem - thanks to the hint in your first reply!

    I was using the same power supply for both the ultrasonic sensor and the motors... I have just fixed up another power supply for the sensor and voila! it works fine now!!

     

    Thank you billabot...

     

      :-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago in reply to billabott

    I have fixed the problem - thanks to the hint in your first reply!

    I was using the same power supply for both the ultrasonic sensor and the motors... I have just fixed up another power supply for the sensor and voila! it works fine now!!

     

    Thank you billabot...

     

      :-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • billabott
    0 billabott over 12 years ago in reply to Former Member

    You are welcome.  Glad I could help.  I will enjoy all 25 of those points too.  image