Arduino
  • Products
  • More
Arduino
Arduino Forum How do I add a Liquid Crystal Display to my current project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 37 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 4688 views
  • Users 0 members are here
  • x
  • 1
  • lcd_display
  • arduino
  • 16
Related

How do I add a Liquid Crystal Display to my current project

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

I recently completed, with some assistance from Coder27, Bill Abbot, Tony, and Mark Beckett the first part of my project ( http://www.element14.com/community/thread/23967?start=0&tstart=0 )

Now the second part - I am wanting to add a small 16 x 1 LCD to finish up my project (see coding below that I will be using)

I would like the LCD to simply show which direction a servo is pointing (as in degrees, such as 0°, 90°, 180°, 270°, or 360° or anywhere in between 0° to 360°)

Please be advised: I do know that arduino 1.0.4 has the LCD Scroll example, but I am sure I dont need the entire code they have.  Also, my LCD is only 16 x 1, not x 2.

Thanks,

~Anna

 

******** BEGINNING OF CODE *************

#include <Servo.h>

 

const int pan1 = 3;     // first servo

const int tilt1 = 5;    // second servo

const int pan2 = 9;     // third servo

const int tilt2 = 11;    // fourth servo

 

const int potpan1 = A0; // Joystick 1 Vertical signal

int val0;

const int pottilt1 = A1;   // Joystick 1 Horizontal signal

int val1;

const int potpan2 = A5;   // Joystick 1 Select signal

int val2;

const int pottilt2= A3;   // Joystick 2 Vertical signal

int val3;

 

int servoVal[4];        // variable to read the value from the analog pin

 

Servo mypan1;                                  // create servo object to control a servo

Servo mytilt1;    // create servo object to control a servo

Servo mypan2;                                  // create servo object to control a servo

Servo mytilt2;    // create servo object to control a servo

 

void setup()

{

 

  // Servo 

  mypan1.attach(pan1);  // attaches the servo

  mytilt1.attach(tilt1);  // attaches the servo

  mypan2.attach(pan2);  // attaches the servo

  mytilt2.attach(tilt2);  // attaches the servo

 

  // Inizialize Serial

  Serial.begin(57600);

}

 

void loop()

{

 

  outputPotentiometers();           // Read and output joystick values

 

  val0 = analogRead(potpan1);            // reads the value of the potentiometer (value between 0 and 1023)

  val0 = map(val0, 0, 1023, 0, 179);     // scale it to use it with the servo (value between 0 and 180)

  mypan1.write(val0);                  // sets the servo position according to the scaled value

 

  //Serial.print("Value of PWM 3:   ");

  //Serial.println(val0);

  //Serial.print("\t");

 

  val1 = analogRead(pottilt1);            // i added

  val1 = map(val1, 0, 1023, 0, 179);     // i added

  mytilt1.write(val1);                  // i added 

 

  //Serial.print("Value of PWM 5:   ");

  //Serial.println(val1);

  //Serial.print("\t");

 

  val2 = analogRead(potpan2);            // i added

  val2 = map(val2, 0, 1023, 0, 179);     // i added

  mypan2.write(val2);                  // i added

 

  //Serial.print("Value of PWM 6:   ");

  //Serial.println(val2);

  //Serial.print("\t");

 

 

  val3 = analogRead(pottilt2);            // i added

  val3 = map(val3, 0, 1023, 0, 179);     // i added

  mytilt2.write(val3);                  // i added

 

  delay(20);                                      

}

 

void outputPotentiometers()     // Display Joystick Values

{

  Serial.print("Pot Pan 1 on ~3:     ");

  Serial.print(analogRead(potpan1));

  Serial.print("\t");

  Serial.print("     Pot Tilt 1 on ~5:     ");

  Serial.print(analogRead(pottilt1));

  Serial.print("\t");

  Serial.print("     Pot Pan 2 on ~9:     ");

  Serial.print(analogRead(potpan2));

  Serial.print("\t");

  Serial.print("     Pot Tilt 2 on ~11:     ");

  Serial.println(analogRead(pottilt2));

  Serial.print("\t");

 

}

 

 

 

********** END OF CODE *************

  • Sign in to reply
  • Cancel

Top Replies

  • ntewinkel
    ntewinkel over 13 years ago +1 suggested
    Here's a good example to start with: http://arduino.cc/en/Tutorial/LiquidCrystal You'd have to change the setup line to be lcd.begin(16,1) for your smaller display (and assuming the lcd lib supports it…
  • mcb1
    mcb1 over 13 years ago in reply to billabott +1 verified
    Annasta Your explanation does give us some clues where your learnng lies, and how you have come to be involved, so thanks. You may have noticed that there are many people asking for help, and a lot are…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to billabott +1
    If I might add a bit to WATB's reply, we get all sorts of questions here, and the kind of answer you want to give differs based on the motivation for the question. If someone is asking for help with what…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    ******* CODING LOCATED AFTER MY "~Anna" *********

     

    So I purchased a Serial LCD (sparkfun PN RTL-09877)

    I hacked some code from Sparkfun’s website and so far so good..well to a point.

    I have attached 2 pics and will need to be used to reference information I am speaking about.

    each column and  row are assigned coordinates by me

    Here are my questions:

    1. 1. What is the opposite of random as seen in lines 43 through 46?
    2. 2. Why am I getting the zeros in PIC # 1: A16 & B16?
    3. 3. Would these same lines cause B1 & B2 to also randomize as seen in pic # 2?
    4. 4. Right now just looking for an answer to this one, its regarding PIC # 3, writing the location to the lcd in degrees.

     

    Note regarding pics.  PIC # 3 are NOT legitimate readings, I added them for the purpose of this question.

     

    To explain further:

     

    As you will see in PIC # 1

    I have programmed the Arduino to write T1: (across A1, A2,& A3)

    I have programmed the Arduion to write T2: (across A9, A10, & A11)

    The information in row B, is the same for the exceptions, B row will be for T2: and P2: respectively.

    So info in these rows and listed columns are to be static.

     

    Now if you would please, focus on A16, and B16 (STILL ON PIC # 1)

    Those 2 zeros, is actually random information (a random generation of info is NOT needed for the project)

    I am pretty sure that the location for this small little glitch will be found in the following lines.

     

    1. Lines 43 through 46 -  I have the RANDOM(1000) listed ß what is the opposite of random?

     

    Now to use PIC # 2

    In this pic we see that the following locations are changing (A16 & B16)

    But notice locations: B1 & B2.  These 2 locations have changed from T2 do randomization.  This one I don’t have a firm grip on but believe its somewhere around the following lines:

    Lines 60 up to 70

     

    Finally PIC # 3

    This is what I need to have showing up.  As in previous postings, I am looking to get the °’s of each pot, when I turn the servo.  My thought process tells me that I need to actually figure out where each given servo is at a certain point of the potentiometer, therefore I would need to have the coding reference the location of the pots. 

     

    1. WOW…ok guys, we are doing so well…I hope you see that I am trying and really attempting things before I post questions…  J

     

     

    ~Anna

     

    ******CODING*********

    LINEPROGRAMMING
    1// SparkFun Serial LCD example 2
    2// Format and display fake RPM and temperature data
    3
    4// This sketch is for Arduino versions 1.0 and later
    5// If you're using an Arduino version older than 1.0, use
    6// the other example code available on the tutorial page.
    7
    8// Use the softwareserial library to create a new "soft" serial port
    9// for the display. This prevents display corruption when uploading code.
    10#include <SoftwareSerial.h>
    11
    12// Attach the serial display's RX line to digital pin 2
    13SoftwareSerial mySerial(3,2); // pin 2 = TX, pin 3 = RX (unused)
    14
    15void setup()
    16{
    17  mySerial.begin(9600); // set up serial port for 9600 baud
    18  delay(500); // wait for display to boot up
    19
    20  mySerial.write(254); // cursor to beginning of first line
    21  mySerial.write(128);
    22
    23  //mySerial.write("RPM:            "); // clear display + legends
    24  //mySerial.write("TEMP:           ");
    25  mySerial.write("T1:     P1:     "); // clear display + legends
    26  mySerial.write("T2:     P2:     ");
    27}
    28
    29//int temp, rpm;
    30//char tempstring[10], rpmstring[10]; // create string arrays
    31int t1, p1, t2, p2;
    32//char t1[8], p1[8], t2[8], p2[8]; // create string arrays
    33char t1string[8];
    34char p1string[8];
    35char t2string[8];
    36char p2string[8];
    37;
    38
    39void loop()
    40{
    41  //temp = random(1000); // make some fake data
    42  //rpm = random(10000);
    43  t1 = random(1000); // make some fake data
    44  p1 = random(1000);
    45  t2 = random(1000); // make some fake data
    46  p2 = random(10000);
    47
    48  //sprintf(tempstring,"%4d",rpm); // create strings from the numbers
    49  //sprintf(rpmstring,"%4d",temp); // right-justify to 4 spaces
    50  sprintf(t1string,"%4d",t1); // create strings from the numbers
    51  sprintf(p1string,"%4d",p1); // right-justify to 4 spaces
    52  sprintf(t2string,"%4d",t2); // create strings from the numbers
    53  sprintf(p2string,"%4d",p2); // right-justify to 4 spaces
    54
    55  //mySerial.write(254); // cursor to 7th position on first line
    56  //mySerial.write(134);
    57  mySerial.write(254); // cursor to 7th position on first line
    58  mySerial.write(143);
    59
    60  //mySerial.write(rpmstring); // write out the RPM value
    61  mySerial.write(t1); // write out the RPM value
    62
    63  //mySerial.write(254); // cursor to 7th position on second line
    64  //mySerial.write(198);
    65  mySerial.write(254); // cursor to 7th position on second line
    66  mySerial.write(207);
    67
    68  //mySerial.write(tempstring); // write out the TEMP value
    69  mySerial.write(t1); // write out the TEMP value
    70  delay(1000); // short delay
    71}

    imageimageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    It is widely known that the HD44780 character ROM includes an ASCII character font (0x00 .. 0x7f)  in addition to a Japanese Katagana charcter font (0x80 .. 0xff).

     

    As the last page of this data sheet shows: http://www.stanford.edu/class/ee281/handouts/lcd_tutorial.pdf

    For a more in depth discussion see: http://symlink.dk/electro/hd44780/

     

    The Maximum value an ASCII user would want returned from a random character generation is 0x7f or 127.

     

    What does that imply for the char = Random(10000); sketch statement?  Since int is a 16 bit storage unit, it can be any unsigned value from zero up to (2^16 -1) = 0xffff.  It would be a good choice to limit the range of the generated value by using the following statement in the sketch:

    char = Random(127); 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to billabott

    I always like it when we spend time helping people, and after 3 or 4 days ........

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to mcb1

    @Mark  are you in a bad mood still?   how is it going at work and home, buddy?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to billabott

    Bill

    On early mornings so getting up early isn't my favourite. ..but thanks

    Trying to get my Pi camera isn't helping ...I need to give up one or the other ....um which one?

     

    No not a bad mood, just annoyed at the time taken by some people to respond to help requests, when I commit my time.

    It doesn't help when suggestions made are ignored.

     

    How is your book review.?

     

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to mcb1

    Okay, I got one for you:  what is the default clock speeds of the attiny45 smd and 8pin dip?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to mcb1

    Thanks for reminding me.  My old iBook is not up to the task of modern iTune standards.  Jeez!  I cannot even download freeduino.begin() with the newest iTunes on my Win7 machine.  DRM restrictions that severe is kinda silly IMHO.  Do you have an iPad with the latest updates?  You are welcome to do the review instead of me.  Say the word and I will suggest your name to the author.

     

    A little bird told me that Annasta is on vacation until after our US Memorial Day, 27 May.

     

    Message was edited by: William Bottger

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to billabott

    billabott wrote:

     

    Okay, I got one for you:  what is the default clock speeds of the attiny45 smd and 8pin dip?

    Good question.

    The Digispark uses the ATtiny85 and will lock it's speed based on the USB connection to 16.5 MHz, but you can apparently set it as low as 1MHz, which of course does wonders for power consumption, but plays havoc with some libraries.

     

    http://digistump.com/board

    I would suggest if you head there, and pose the question, I'm sure you'll get an answer.

     

    For those not familiar, the Digispark is a mini arduino that uses a modified IDE to program an ATtiny85, and with some clever bootloading, allows the 6 I/O pins to be used, including the 2 pins used to communicate to the USB.

    http://digistump.com/category

    While lacking some features, it will present as a USB device, something most arduino can't.

     

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 13 years ago in reply to billabott

    billabott wrote:

     

    Okay, I got one for you:  what is the default clock speeds of the attiny45 smd and 8pin dip?

    Good question.

    The Digispark uses the ATtiny85 and will lock it's speed based on the USB connection to 16.5 MHz, but you can apparently set it as low as 1MHz, which of course does wonders for power consumption, but plays havoc with some libraries.

     

    http://digistump.com/board

    I would suggest if you head there, and pose the question, I'm sure you'll get an answer.

     

    For those not familiar, the Digispark is a mini arduino that uses a modified IDE to program an ATtiny85, and with some clever bootloading, allows the 6 I/O pins to be used, including the 2 pins used to communicate to the USB.

    http://digistump.com/category

    While lacking some features, it will present as a USB device, something most arduino can't.

     

     

    mark