Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Sketch Question???
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 419 subscribers
  • Views 704 views
  • Users 0 members are here
  • i/o
  • expected_declaration_before_'}'_token
  • help
  • buggy
  • sketch
  • io
  • expected_unqualified-id_before_'else'
  • code
  • bug
  • error
  • arduino
  • question
Related

Arduino Sketch Question???

fechrxy
fechrxy over 13 years ago

Hey, can anyone tell me why i am getting this error in my code as opposed to this other guy's code which is very similar?

I uploaded pictures of the bottom half of the code but i can provide additional information if needed. 

I would love to know how to fix the error,  Thanks!

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • ntewinkel
    ntewinkel over 13 years ago +1
    I can't really tell without the rest of the code, but first thing to check is to make sure RELAY is defined somewhere.
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to billabott +1
    > does not allow me or others to put the sketch into our arduino IDE and compile the sketch . where's the sport in that?
  • fechrxy
    fechrxy over 13 years ago +1
    Hey guys, i'm really sorry i did'nt upload the full sketch however i did fix the prblem by deleting all of my notes in the sketch. Thanks so much for your feedback. Cheers!
Parents
  • billabott
    0 billabott over 13 years ago

    What version of Arduino hardware are you using?  Which digital pin that supports PWM is the Relay connected to?

     

    Are we to assume that your relay is connected as the standard LED?  and will only draw 20 mA or less and have diode protection from back EMF?  not to mention the need for pullup resistor of the proper value; internal or external!

     

    int ledPin = 13;                 // LED connected to digital pin 13


    void setup()

    {

      pinMode(ledPin, OUTPUT);      // sets the digital pin as output

    }

     

    One more note: Providing a .jpg image of a sketch segment does not allow me or others to put the sketch into our arduino IDE and compile the sketch.  I am just not that interested in retyping some sketch.  Only a complete sketch would be suitable for testing changes that may solve the difficulty.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago

    What version of Arduino hardware are you using?  Which digital pin that supports PWM is the Relay connected to?

     

    Are we to assume that your relay is connected as the standard LED?  and will only draw 20 mA or less and have diode protection from back EMF?  not to mention the need for pullup resistor of the proper value; internal or external!

     

    int ledPin = 13;                 // LED connected to digital pin 13


    void setup()

    {

      pinMode(ledPin, OUTPUT);      // sets the digital pin as output

    }

     

    One more note: Providing a .jpg image of a sketch segment does not allow me or others to put the sketch into our arduino IDE and compile the sketch.  I am just not that interested in retyping some sketch.  Only a complete sketch would be suitable for testing changes that may solve the difficulty.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    > does not allow me or others to put the sketch into our arduino IDE and compile the sketch.

     

    where's the sport in that?