Arduino
  • Products
  • More
Arduino
Arduino Forum problem with digital input pins in controlling its output pins.. we really need suggestions...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 418 subscribers
  • Views 733 views
  • Users 0 members are here
Related

problem with digital input pins in controlling its output pins.. we really need suggestions...

e14 Contributor
e14 Contributor over 13 years ago

i have 2 digital input pins(pin16 & pin17 actually i need 4)

just to test if it really gonna work.What i did is that

i just give 5volts or high to these pins as input data

but what happened there is that the 2 digitalOutput pins respectively

seems doesnt do to the conditions i gave it seems it can affect the other condition.

 

 

here is a part of my code .

 

  if (digitalRead(16) == LOW )

    { digitalWrite(ledPin7,HIGH);

    }

  if (digitalRead(17) == LOW )

    { digitalWrite(ledPin6,HIGH);

    }

 

  else

    digitalWrite(ledPin7,LOW);

    digitalWrite(ledPin6,LOW);

 

          ,,

          what i really want to do there is that

          just have  4  inputs(that would be 5volts)

          and also give 4  outputs respectively..

 

we really need Ur suggestions  and ideas.. thnx ;d

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 13 years ago in reply to billabott +2
    Nico Well done One other way is to make them LOW and change them if the button is LOW. digitalWrite(ledPin7,LOW); digitalWrite(ledPin6,LOW); if (digitalRead(16) == LOW ) { digitalWrite(ledPin7,HIGH); …
  • ntewinkel
    ntewinkel over 13 years ago +1 suggested
    I think it might be the way you are building your if...else statements. Try this way: if (digitalRead(16) == LOW ) { digitalWrite(ledPin7,HIGH); } else { digitalWrite(ledPin7,LOW); } if (digitalRead(17…
  • billabott
    billabott over 13 years ago in reply to ntewinkel +1
    Arduino IDE is modified version of the Processing Application as specified on Processing.org. (Think Turtle programming) My question is a carry over tangent from the J.Blum Arduino discussion.
Parents
  • billabott
    0 billabott over 13 years ago

    I like this.  It is really much better to start a new discussion and it would be a good idea to now delete that old original duplicate post.

     

    I did make a suggestion.  Did you not see it?  It has been removed now.

     

    Here it is again.

     

    Seems to me that what you require is an 8 bit (4 inputs plus 4 outputs) I2C i/o expander chip.

     

    They are frequently used to take the 8 minumum required inputs of a standard 2x16 LCD and convert it to Serial LCD.  The I2C LCD can be seen on eBay and wherever other fine electronics parts are sold.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago

    I like this.  It is really much better to start a new discussion and it would be a good idea to now delete that old original duplicate post.

     

    I did make a suggestion.  Did you not see it?  It has been removed now.

     

    Here it is again.

     

    Seems to me that what you require is an 8 bit (4 inputs plus 4 outputs) I2C i/o expander chip.

     

    They are frequently used to take the 8 minumum required inputs of a standard 2x16 LCD and convert it to Serial LCD.  The I2C LCD can be seen on eBay and wherever other fine electronics parts are sold.