Arduino
  • Products
  • More
Arduino
Arduino Forum Sensing Velocity for MIDI using Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 418 subscribers
  • Views 2068 views
  • Users 0 members are here
Related

Sensing Velocity for MIDI using Arduino

bnelson218
bnelson218 over 13 years ago

Hello,

My name's Bruce and I have both programming (Visual Basic) and electronics experience, but no experiance with Arduino. My quest here is to find a way to use force sensing resistor strips and Arduino to obtain and send velocity sensitivity data to a MIDI controller. If unfamiliar, MIDI stands for Musical Instrument Digital Interface and represents a language through which musical instruments, namely synthesizers, can communicate with each other (although it has been expaned greatly since its inception in the early '80s). Velocity sensitivity refers to, for instance, how hard a pianist strikes the key--the harder it is struck the louder the note sounds. In the digital world, such as with digital pianos, key contacts are used, one closing slightly before the other, and thereby producing a differential which is then calculated and transferred to velocity data thus sounding the note at the appropriate amplitude. Through a Google search I came across a fellow (I believe it was the HackADay.com site) who used resistive force strips in conjunction with an Arduino processor to calculate and transmit the velocity data to his MIDI processor. Unfortunately, the fellow won't return any of my inquiries so I am exploring other avenues. My ultimate goal is to come up with a system that will work beneath the keys of a Hammond organ, such as a B3 or C3. Due to the amount of space available beneath the keys--5mm when a key is pressed--switch contacts are absolutely out of the question. The force-sensing strips I've seen, such as pololu.com's item #1697, seem perfect for the job. They are 24" long (so 2 would be needed to cover a 61-note keyboard) and would fit perfectly under the keys. All I have to do now is figure out the rest of the puzzle.  image

So, if anyone has any thoughts on this, or perhaps needs more info, I would appreciate hearing from you.

Regards,

Bruce Nelson

bnelson218@yahoo.com

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Bruce, do you already have a key-on/key-off system in place? Or in simpler terms, a key-press detection system without any velocity detection?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bnelson218
    0 bnelson218 over 13 years ago in reply to e14 Contributor

    Hi,

    Yes, there's a system in place in case I can't develop the VS ability. It's a VS-capable midi controller board made by midiboutique.com, model MKCV128SN, which offers 128-note capability. The nice thing with this company is that at time of purchase I can describe the various functions I need (in my case this'll include octave up and down switches, a level control, and Pitch amd Mod' wheels) and they'll burn the processor with these options. So I'm assuming they can also burn in whatever's needed to accept VS data from an Arduino/force resistor circuit. The only thing that's bugging me is what I'm calling the release factor. Perhaps hard to explain if you're not a keyboard player, but I'm assuming that if I press a key, and the Arduino circuit reads and sends the key's velocity data, will that key need to be released before VS data can be read again? I'm guessing so and this may cause problems if you're plating arpeggios that require the notes to be held

    down as succesive note are added. Like I said, it's a little hard to explain to non players, but if you do play keyboards then you can likely imagine what I'm getting at. The VS data for the first key played will likely establish the VS for any subsequent keys played if the first key is not released.

     

    This fellow has done exactly what I'd like to do, using 4 force resistor strips under a toy keyboard, probably to establish some independeny along the keyboard in dealing with the situation I descibed above. Actually, since these strips can be cut to specific lengths, couldn't I do one for each key?

    Here's a YouTube video by a guy named Jen Shen who's installed the force resistor strips in a toy keyboard and achieved not only velocity sensitivity but also after touch:

    http://www.youtube.com/watch?v=yIBBxDHOa0g

     

    Once a key is held down, after touch allows the player to alter the sound by changing the pressure on the key.

     

    Here's Jen's Jen's tutorial on cutting the strips:

    http://www.youtube.com/watch?v=x-pQ651_iZY

     

    By the way, this is the same fellow I saw originally that lead me to the idea of using these strips, unfortunately he won't answer any of my inquiries--probably inundated with emails and busy. Go figure. There's a ton of info on this. On Google I searched "midi velocity diy arduino" and got all kinds of returns, but not being familiar with Arduino and tghe associated verbage I could very well be looking at exactly what I need and not know it. Arrrg...

     

    Well, I appreciate your interest in this and hope you can assist me in making it work.

    Best regards,

    Bruce Nelson

    Toledo, OH

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bnelson218

    Hello there Bruce, I understand a little bit of keyboard playing, so I can perfectly understand what you're getting at! image. I'm not entire sure if I can help you, but here is my two cents about the subject;

    I'm familiar with the project that you've linked, did you've checked the blog post about it? in it you can have a schematic and even a part-list. The main problem is that for every Velocity/Aftertouch detector, you'll have to expend an average of 4$. He uses those "slide" pads that i'm sure you're familiar with. So, I'm not sure this is the way to go, if you're looking for a keyboard with a decent amont of keys.

     

    I'm not entirely sure if I will help you or confuse you even more, but here it goes.

    The reason why I've asked if you already have a "Note-On/Off" system in place, is because for velocity calculation you would simply have to duplicate it. You would put two pressure pads on each key, one would be activated if the key is just touched and the other only when the key is fully pressed. Using an Arduino you would then calculate the delay between the two Inputs and have the "Velocity".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to e14 Contributor

    Not to barge in on your conversation.....

     

    Would an accelerometer be of any use.?

    It will detect the force of the key hitting home and transfer that into a 'z' axis.(up/down)

    You know what key and from the accelerometer, how much force was applied.

     

    At worst you might need three to cover the whole organ more evenly.

     

    I wouldn't have thought this was possible, until I ran across the "secret knock' example on mbed.org using a KL25z board.

    With a setting of about 1/2 g the knock on the table is not at all loud, so the sensitivity is there.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 13 years ago in reply to e14 Contributor

    Not to barge in on your conversation.....

     

    Would an accelerometer be of any use.?

    It will detect the force of the key hitting home and transfer that into a 'z' axis.(up/down)

    You know what key and from the accelerometer, how much force was applied.

     

    At worst you might need three to cover the whole organ more evenly.

     

    I wouldn't have thought this was possible, until I ran across the "secret knock' example on mbed.org using a KL25z board.

    With a setting of about 1/2 g the knock on the table is not at all loud, so the sensitivity is there.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bnelson218
    0 bnelson218 over 13 years ago in reply to mcb1

    Hi Mark,

     

    You're not barging at all as I am anxious for replies. I'm not familiar with accelerometers such as size or height, so it's hard to know if they'd work or not. How would it sense the key's movement?

     

    Thanks,

    Bruce

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to bnelson218

    Bruce

    3 axis accelerometers are used in smartphones, nintendo Wii, and lots of other things.

    They range in size, but are only 3-4mm square.

    http://nz.element14.com/freescale-semiconductor/mma8453qt/accelerometer-10-8bit-3axis-16qfn/dp/1842361

     

    NZ link but probably the same part number in other E14 stores.

    Sparkfun have a similar on a breakput board (ie soldered onto a board) https://www.sparkfun.com/products/9652

     

    Basically you fit them onto the organ and they will detect movement in relation to their position.

    With a thump of the key it will translate into a Z axis (vertical).

     

     

    This relies on the ability to detect which key has been pressed, which I thought you were able to do from the key contact that drives the organ.

    Maybe I missed that ....

     

     

    Mark