Arduino
  • Products
  • More
Arduino
Arduino Forum Developing Arduino Shields with an FPGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 418 subscribers
  • Views 982 views
  • Users 0 members are here
  • cyclone
  • fpga
  • shield
  • altera
  • arduino
  • module
Related

Developing Arduino Shields with an FPGA

e14 Contributor
e14 Contributor over 13 years ago

Here's a campaign on IndieGoGo for an FPGA system that drives 3x UNO shields. http://igg.me/at/fpga-module/x/3703559

A good system? Worth supporting?

 

Your thoughts...?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 13 years ago +1
    For hobby use maybe .... but it's a lot of money for the full kit. For pro use - no chance .... when I want to design in an FPGA I scope the system, decide on the FPGA (based on the task, production numbers…
  • johnbeetem
    johnbeetem over 13 years ago in reply to michaelkellett +1
    Michael Kellett wrote: I also think that the IndieGoGO site over-hypes the use of FPGAs, System Verilog is most certainly not much like C (get your head round begin/end, fork/join for starters) and programming…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to michaelkellett +1
    Hi MK, It sounds like you have volume in your projects. helix_4 is meant to appeal if you *don't* have much volume. When your volumes are <100pcs you don't get play from Distributors or Vendors or assembly…
Parents
  • michaelkellett
    0 michaelkellett over 13 years ago

    For hobby use maybe .... but it's a lot of money for the full kit.

     

    For pro use - no chance .... when I want to design in an FPGA I scope the system, decide on the FPGA (based on the task, production numbers, customer preferences etc) and then I design a board. (Might not do all these things myself if it's a big job).

    There is no way I would use a little solder in type module when I can get free standing dev boards from the FPGA companies (if I want them) at anyhting from free ( as in beer) upwards.

     

    I also think that the IndieGoGO site over-hypes the use of FPGAs, System Verilog is most certainly not much like C (get your head round begin/end, fork/join for starters) and programming an FPGA in SV is a very different task from writing  code for an Arduino or a micro in C. (I'm not saying that it can't be done for fun, just that it's a different kind of fun !).

     

    I think most hobby types would do better to look at one of the little (and cheap) FPGA shields or the FPGA add on for the RPi.

     

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to michaelkellett

    Hi MK, It sounds like you have volume in your projects.

     

    helix_4 is meant to appeal if you *don't* have much volume. When your volumes are <100pcs you don't get play from Distributors or Vendors or assembly houses.  If X and A won't give you free boards, and they won't give you hot volume pricing, how do you make it happen? We know we're not going to appeal for projects with >100pcs, but if you are doing 10 or 20 - a nice short run - then a $40~60 module covered in RAM that saves you 3 BGA placements and the yield issues... hoping that appeals to someone.

     

    A lot of people are comparing us to Papillio, and that's a good thing- great product. We differentiated ourselves:

     

    1) For the dev board we didn't make an accessory board standard of our own, or use IDE hdrs - we hooked into the Ardunio UNO shields because there are 300+, they are very good generally, lots of OSHW & code, and lots of vendors develop them.

    2) We give you the option to make a 2 layer board and use the module. This can get you a NICE finished product, that is the right form factor and fits a standard case or one you've 3d printed. I pay $55 for 10pcs of a 2 layer board, so cheap that we think this is the way prototyping will go - fewer wires and kluge, more quick spin PCBs with modules.

    3) The specs are different. We're a bit higher spec: 8x more dram,and its ddr2, 22kle vs 9kle, sram that runs @ 50mhz, the atsha204 crypto chip, similar io count. the papilio has more flash, and has an integrated programmer, but we didn't embedd a programmer because they are cheap enough, and we want our customers to end up on a bespoke 2 layer board, so they'd need to take the programmer dongle to that board eventually. We're considering bunding a programmer dongle - but need more feedback first.

     

    Thanks for the time to look at the campaign and make comment. Your feedback is gold.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to michaelkellett

    Hi MK, It sounds like you have volume in your projects.

     

    helix_4 is meant to appeal if you *don't* have much volume. When your volumes are <100pcs you don't get play from Distributors or Vendors or assembly houses.  If X and A won't give you free boards, and they won't give you hot volume pricing, how do you make it happen? We know we're not going to appeal for projects with >100pcs, but if you are doing 10 or 20 - a nice short run - then a $40~60 module covered in RAM that saves you 3 BGA placements and the yield issues... hoping that appeals to someone.

     

    A lot of people are comparing us to Papillio, and that's a good thing- great product. We differentiated ourselves:

     

    1) For the dev board we didn't make an accessory board standard of our own, or use IDE hdrs - we hooked into the Ardunio UNO shields because there are 300+, they are very good generally, lots of OSHW & code, and lots of vendors develop them.

    2) We give you the option to make a 2 layer board and use the module. This can get you a NICE finished product, that is the right form factor and fits a standard case or one you've 3d printed. I pay $55 for 10pcs of a 2 layer board, so cheap that we think this is the way prototyping will go - fewer wires and kluge, more quick spin PCBs with modules.

    3) The specs are different. We're a bit higher spec: 8x more dram,and its ddr2, 22kle vs 9kle, sram that runs @ 50mhz, the atsha204 crypto chip, similar io count. the papilio has more flash, and has an integrated programmer, but we didn't embedd a programmer because they are cheap enough, and we want our customers to end up on a bespoke 2 layer board, so they'd need to take the programmer dongle to that board eventually. We're considering bunding a programmer dongle - but need more feedback first.

     

    Thanks for the time to look at the campaign and make comment. Your feedback is gold.