Arduino
  • Products
  • More
Arduino
Arduino Forum Ethernet problem sending null characters
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 418 subscribers
  • Views 2920 views
  • Users 0 members are here
  • client
  • client.print
  • ethernet
  • client.write
Related

Ethernet problem sending null characters

e14 Contributor
e14 Contributor over 13 years ago

Thank you in advance for your kind help.

I am using the Ethernet Library (client.print function) to access an electronic device which supports TCP/IP.

I must send a command string to the device that contains several NULL characters. I cannot send the string since the first NULL character terminates the transmission.

I tried sending 1 byte at a time and that works when sent to a VB.NET simulator that I wrote, however, it doesn't work with the device I am trying to use. I think the device may be expecting the entire command to be contained in a single packet. I tried using a string object and that didn't work either.

I need to be able to specify the data and its length and send it as a single packet.

Can anyone out there help me ?

Thanks,

Nick

Attachments:
EthernetCode.txt.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1 +1
    Mark, I haven't tried with firefox, but I doubt that would make a difference. Be sure to copy & paste the quoted material first into your draft post before highlighting it in the draft, and then clicking…
  • billabott
    billabott over 13 years ago +1
    make a quote out of something you paste into a message, you don't have to quote the previous message, then delete everything in the quote, and then paste into the empty quote. In Firefox, the e14 UI Editor…
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor +1
    Be sure to copy & paste the quoted material first into your draft post before highlighting it in the draft, and then clicking the "quote" icon. Are that be the difference ..... I wasn't pasting it in and…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    It appears that my initial post somehow got changed into a discussion of how to cut and past.

     

    I hope you all can agree on how to use this forum but I was expecting a bit more Arduino expertise.

     

    Nick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    You are correct, Nick.  Since, I am not inclined to open any zip file.  I will pose some questions to you.  What is the device you are communicating with?  What is it supposed to DO when the string of nulls is detected?  Is it hanging up when the single null arrives?  Which process or hardware is breaking the (TCP?) connection?

    Is there an escape character(s) that will allow the string of nulls to get all the way thru to the device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    You are correct, Nick.  Since, I am not inclined to open any zip file.  I will pose some questions to you.  What is the device you are communicating with?  What is it supposed to DO when the string of nulls is detected?  Is it hanging up when the single null arrives?  Which process or hardware is breaking the (TCP?) connection?

    Is there an escape character(s) that will allow the string of nulls to get all the way thru to the device.