Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Sketch Question?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 416 subscribers
  • Views 486 views
  • Users 0 members are here
  • i/o
  • source_code
  • buttons
  • loop
  • sketch
  • program
  • programming
  • code
  • array
  • arduino
Related

Arduino Sketch Question?

fechrxy
fechrxy over 13 years ago

So I have a sketch that using an array, digitally reads five pins connected to buttons then writes to the serial monitor whethor or not they are on or off. But when i turn the switch on or off it won't just write On/Off once it will write it alot of times because its part of a loop. Does any one know how to make the sketch below only print On/Off once or basically how to make something not loop in a loop? Maybe with a boolean? Sorry i ask so many questions, thanks!

 

 

 

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to fechrxy +1
    Tony, You have LastButtonState[ThisPin] = ButtonState[ThisPin]; in the "else" part, but it looks like you should be setting LastButtonState regardless of whether ButtonState is HIGH or LOW. That would…
Parents
  • ntewinkel
    0 ntewinkel over 13 years ago

    Hi Tony!

     

    No worries, I think questions are a big reason these forums exist image

     

     

    I don't see your sketch attached, but to show a status change only once in a loop you can keep a variable that holds the latest status, and if it's different from the current status, print the message and update the variable.

     

    kinda like this (loosely based on the Button example)...

     

    int lastbuttonstate = 0;

    int newbuttonstate = 0;

     

    loop {

     

      newbuttonstate = digitalRead(buttonPin); // probably needs some debouncing

        

       if (newbuttonstate != lastbuttonstate) {  

     

         if (newbuttonstate == HIGH) {

              Serial.println("ON");

          }

          else {

              Serial.println("OFF");

         }

     

         lastbuttonstate = newbuttonstate;

       }

     

    }

     

    I think that will do the trick!

     

    ps, how did your relay project turn out?

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fechrxy
    0 fechrxy over 13 years ago in reply to ntewinkel

    Thanks for the response! I put in your code and this is definitely the closest it has been to working. However it still has a few problems like when I hit/hold any one of the buttons it says "on on on on on on" and when I release the button it does not say off. Those are the only issues I can foresee at the moment so if you know of any fix for them I would love to hear it. And my relay project is going great! I am almost ready to install  the project into my home lighting system. Thanks so much for all your help!

     

     

    static byte ButtonPins[5] = {2, 3, 4, 5, 6};

    const int PinCount = (5);

    int ThisPin;

     

     

    void setup()

    {

      Serial.begin(9600);

     

      for (ThisPin = 0; ThisPin < PinCount; ThisPin++)

      {

      pinMode(ButtonPins[ThisPin], INPUT); 

      }

    }

     

     

     

     

    void loop()

    {

    static byte ButtonState[PinCount];

    static byte LastButtonState[PinCount];

     

    for (ThisPin = 0; ThisPin < PinCount; ThisPin++)

    {

      ButtonState[ThisPin] = (digitalRead(ButtonPins[ThisPin]));

     

    if (ButtonState[ThisPin] != LastButtonState[ThisPin])

      {

     

    if (ButtonState[ThisPin] == HIGH)

        {

      Serial.println(ThisPin, DEC);

      Serial.println(" ON");

      }

        

    else

       {

       Serial.println(ThisPin, DEC);

       Serial.println(" OFF");

       LastButtonState[ThisPin] = ButtonState[ThisPin];

       }

       }

       }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fechrxy
    0 fechrxy over 13 years ago in reply to ntewinkel

    Thanks for the response! I put in your code and this is definitely the closest it has been to working. However it still has a few problems like when I hit/hold any one of the buttons it says "on on on on on on" and when I release the button it does not say off. Those are the only issues I can foresee at the moment so if you know of any fix for them I would love to hear it. And my relay project is going great! I am almost ready to install  the project into my home lighting system. Thanks so much for all your help!

     

     

    static byte ButtonPins[5] = {2, 3, 4, 5, 6};

    const int PinCount = (5);

    int ThisPin;

     

     

    void setup()

    {

      Serial.begin(9600);

     

      for (ThisPin = 0; ThisPin < PinCount; ThisPin++)

      {

      pinMode(ButtonPins[ThisPin], INPUT); 

      }

    }

     

     

     

     

    void loop()

    {

    static byte ButtonState[PinCount];

    static byte LastButtonState[PinCount];

     

    for (ThisPin = 0; ThisPin < PinCount; ThisPin++)

    {

      ButtonState[ThisPin] = (digitalRead(ButtonPins[ThisPin]));

     

    if (ButtonState[ThisPin] != LastButtonState[ThisPin])

      {

     

    if (ButtonState[ThisPin] == HIGH)

        {

      Serial.println(ThisPin, DEC);

      Serial.println(" ON");

      }

        

    else

       {

       Serial.println(ThisPin, DEC);

       Serial.println(" OFF");

       LastButtonState[ThisPin] = ButtonState[ThisPin];

       }

       }

       }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to fechrxy

    Tony,

        You have

           LastButtonState[ThisPin] = ButtonState[ThisPin];

    in the "else" part, but it looks like you should be setting

    LastButtonState regardless of whether ButtonState is HIGH or LOW.

     

    That would involve just moving it down a line after the first "}",

    like Nico's code.  You also probably want to initialize LastButtonState

    to 0, like Nico showed.