Arduino
  • Products
  • More
Arduino
Arduino Forum question in xbee+lcd
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 418 subscribers
  • Views 517 views
  • Users 0 members are here
Related

question in xbee+lcd

e14 Contributor
e14 Contributor over 13 years ago

i was connecting a netwrok that works like this

 

1.xbee transmitter connectedc to a laptop

2.xbee connected to arduino

3.kcd connected to arduino

 

* both xbee are talking with each other accept one thing ; when the xbee connected to the arduino then the reciever gets the ascii notes a-g as 255 instead of thir real values and q-z also as 255 instead of the real value

 

how to fix this?

 

my code is such :

 

#include  <LiquidCrystal.h>

 

LiquidCrystal lcd (12,11,5,4,3,2);

 

void steup () {

 

lcd.begin(16,2);

Serial.begin(9600);

lcd.setCursor(0,0);

}

 

void loop() {

 

if (Serial.available() > 0 ) {

 

char (temp) = Serial.read() ;

lcd.print(temp) ;

}

}

 

ay ideas? i can see the notes h-p but thats it!...

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi mark i copied it by hand not copy paste so i guess i did void setup(){  anyway thats not the problem the problem is the recieving xbee reads correctly the ascii notes h-o the rest he sees as 255 which is a nothing!  All the notes and there all 255 ascii to him...why? How to resolve this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi mark i copied it by hand not copy paste so i guess i did void setup(){  anyway thats not the problem the problem is the recieving xbee reads correctly the ascii notes h-o the rest he sees as 255 which is a nothing!  All the notes and there all 255 ascii to him...why? How to resolve this?