Arduino
  • Products
  • More
Arduino
Arduino Forum question in xbee+lcd
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 418 subscribers
  • Views 513 views
  • Users 0 members are here
Related

question in xbee+lcd

e14 Contributor
e14 Contributor over 13 years ago

i was connecting a netwrok that works like this

 

1.xbee transmitter connectedc to a laptop

2.xbee connected to arduino

3.kcd connected to arduino

 

* both xbee are talking with each other accept one thing ; when the xbee connected to the arduino then the reciever gets the ascii notes a-g as 255 instead of thir real values and q-z also as 255 instead of the real value

 

how to fix this?

 

my code is such :

 

#include  <LiquidCrystal.h>

 

LiquidCrystal lcd (12,11,5,4,3,2);

 

void steup () {

 

lcd.begin(16,2);

Serial.begin(9600);

lcd.setCursor(0,0);

}

 

void loop() {

 

if (Serial.available() > 0 ) {

 

char (temp) = Serial.read() ;

lcd.print(temp) ;

}

}

 

ay ideas? i can see the notes h-p but thats it!...

  • Sign in to reply
  • Cancel
Parents
  • dmaruska
    0 dmaruska over 13 years ago

    What pins are the LCD and xbee on when connected to the Arduino?

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dmaruska
    0 dmaruska over 13 years ago in reply to dmaruska

    I made a change to your code and ran on simulator.  simulator works ok with this, but crashes on your code.

     

     

    #include <LiquidCrystal.h>

    LiquidCrystal lcd (12,11,5,4,3,2);

     

    void setup()

    {

    lcd.begin(16,2);

    Serial.begin(9600);

    lcd.setCursor(0,0);

    }

    void loop()

    {

    if (Serial.available())

    {

    delay(250);

    lcd.clear();

    while (Serial.available() > 0 )

    {

    //char(temp) = Serial.read();

    //lcd.print(temp);

    lcd.write(Serial.read());

    }

    }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to dmaruska

    hi there thanks for the reply

     

    but it didnt work...it still says that all the other notes in the kwyboard apart h-o are 255 ascii code which means a blank square

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to dmaruska

    hi there thanks for the reply

     

    but it didnt work...it still says that all the other notes in the kwyboard apart h-o are 255 ascii code which means a blank square