Arduino
  • Products
  • More
Arduino
Arduino Forum Uno + 4 Wire Stepper Motor + 12V Power Supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 416 subscribers
  • Views 434 views
  • Users 0 members are here
  • stepper
  • uno
  • motor
  • arduino
Related

Uno + 4 Wire Stepper Motor + 12V Power Supply

e14 Contributor
e14 Contributor over 13 years ago

Hello, I currently have a NEMA 17 stepper motor with an EasyDriver hooked up to an Arduino Uno with a 12 Volt power supply. Eventually, we are going to attach a load cell with a strain meter and will want to have the force to always be at 8 lbs. The stepper motor will be coupled with a vertical stage dial that will rotate depending on if the force is above or below 8 lbs. As of right now, I was wondering if it is possible to code the arduino to turn the stepper motor "counter clockwise" if the 12V power supply is under 12V and "clockwise" if it is over 12V just to practice for when the strain meter comes in. Is there a way for the arduino to read how many volts are output from the power supply? That is where I'm stuck right now. Thanks!

  • Sign in to reply
  • Cancel
Parents
  • colecago
    0 colecago over 13 years ago

    Use a voltage divider on one of the ADC's to get a voltage in the range your Arduino can read (3.3V or 5V depending on your Arduino).  Basically two resistors in series between 12V and ground and you take your signal in the middle between the two resistors. 

     

    Vout = 12V * R2/(R1 + R2)  (with R2 being the resistor tied to ground)

     

    You should add a capacitor to that ADC line to get down some of the power supply noise as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • colecago
    0 colecago over 13 years ago

    Use a voltage divider on one of the ADC's to get a voltage in the range your Arduino can read (3.3V or 5V depending on your Arduino).  Basically two resistors in series between 12V and ground and you take your signal in the middle between the two resistors. 

     

    Vout = 12V * R2/(R1 + R2)  (with R2 being the resistor tied to ground)

     

    You should add a capacitor to that ADC line to get down some of the power supply noise as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer