Arduino
  • Products
  • More
Arduino
Arduino Forum Piano Stairs (Musical Stairs) Part 1 - Planning and feasibility
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 420 subscribers
  • Views 2218 views
  • Users 0 members are here
Related

Piano Stairs (Musical Stairs) Part 1 - Planning and feasibility

e14 Contributor
e14 Contributor over 13 years ago

I would like to turn my basement stairs into "piano stairs". This is a request for input more than a show and tell.
 
Background:
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Project stairs:

http://img.photobucket.com/albums/v112/prn_star/piano%20stairs/IMG_1752.jpg

Stairs from underneath.

http://img.photobucket.com/albums/v112/prn_star/piano%20stairs/IMG_1754.jpg

~Specs:

http://img.photobucket.com/albums/v112/prn_star/piano%20stairs/Untitled.jpg

 

I have purchased nothing yet.

Item starter list:

Raspberry Pi

Ardunio (max) (I would like 12 "keys" or active stairs min)

sensors - tbd

 

The sensing is going to be the hard part (I think):

 

FSR: I started looking into force sensing resisters to be put under the laminate flooring but from googling and reading I'm uncertain that would work well.

 

PIR motion sensors issues/questions:

From looking on youtube most of the PIR sensors either have 2 short a sensing range or too large a range. 10cm to 15cm would probably be idea.

The "reset" time on PIR's factory preset?

If someone tried to key a stair twice quickly it would probably not activate for 2+ seconds?

 

IRDS: Thoughts on using IR distance sensor instead of PIR?

IR has the right range settings from 4 inches (10 cm) to 80cm.

 

IR Beam: Beam sensor would be too difficult to install due to the physical requirements of access to both sides of the stairs.

 

I'm assuming that I can get the sensed activation from the Ardunio to the rPI to play a note or tone?

Would this setup be able to trigger multiple notes at once? Lets say 4 feet(2 people) playing.

 

Thoughts on if this project is worthwhile?

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 13 years ago +1
    Cool idea I remember something similar in a night club mannnnny years ago, and it worked great....except when everyone stood on the stairs. You might want to look at capacitive sensing. You basically stick…
Parents
  • billabott
    0 billabott over 13 years ago

    Hi.  Do you like the auditory effects of the saw tooth wave?  I stumbled across an analog circuit that generates a saw tooth output using a schottky diode.  I am wondering if a VariCap Diode could be used in the circuit in lieu of a regular capacitor.  My idea is to have the arduino set the capacitance (tone control = f of note)  with one digital output pin ( if PWM cannot control the VariCap input then a resistor ladder might have to be used ) and turn the note on/off with another another digital output pin.  I will put a circuit diagram if needed, but it consists of  the Cap and Schockley in parallel up from ground, output tapped off at top of cap and a series resistor to set the max. current.       Output feeds Op-amp - Low Pass filter  - Op-amp - Speaker  ??

       _/|/|/|/|/|/|/|/|_

     

    The triangle wave is much more pleasant to the ear.  It can be generated with an additional resistor in series with the Schockley diode.  Resistor2 and S.diode in series will then be in parallel with the Cap/VariCap.

     

    __/\/\/\/\/\/\/\/\__

     

    image Looks like VariCaps are VHF devices and not AF devices.  Maybe someone smarter than I can figure out how to extract the audio freq. differential with the application of a FM detector or something else. 

     

    Lots of other ways to gen a triangle wave especially using op-amps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago

    Hi.  Do you like the auditory effects of the saw tooth wave?  I stumbled across an analog circuit that generates a saw tooth output using a schottky diode.  I am wondering if a VariCap Diode could be used in the circuit in lieu of a regular capacitor.  My idea is to have the arduino set the capacitance (tone control = f of note)  with one digital output pin ( if PWM cannot control the VariCap input then a resistor ladder might have to be used ) and turn the note on/off with another another digital output pin.  I will put a circuit diagram if needed, but it consists of  the Cap and Schockley in parallel up from ground, output tapped off at top of cap and a series resistor to set the max. current.       Output feeds Op-amp - Low Pass filter  - Op-amp - Speaker  ??

       _/|/|/|/|/|/|/|/|_

     

    The triangle wave is much more pleasant to the ear.  It can be generated with an additional resistor in series with the Schockley diode.  Resistor2 and S.diode in series will then be in parallel with the Cap/VariCap.

     

    __/\/\/\/\/\/\/\/\__

     

    image Looks like VariCaps are VHF devices and not AF devices.  Maybe someone smarter than I can figure out how to extract the audio freq. differential with the application of a FM detector or something else. 

     

    Lots of other ways to gen a triangle wave especially using op-amps.