Arduino
  • Products
  • More
Arduino
Arduino Forum Which is better Input 5 volts to arduino..??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 420 subscribers
  • Views 2213 views
  • Users 0 members are here
Related

Which is better Input 5 volts to arduino..??

e14 Contributor
e14 Contributor over 13 years ago

Guys, I intend to use arduino 24*7. I'm using it in a small industrial bot. I don't want my arduino to draw a higher current than its capability and get damaged. In my application I use 5 digital pins of my arduino as input n rest as output. To make sure OUTPUT pins does not draw more current, I've conneted it to ULN 2803 which is having further connections. I'm okay in that. I want to ask, would it be better to give the input 5 volts to the INPUT pins in my code from the "5V pin of arduino" or "from my 5 Volt regulator IC 7805". My goal is to make sure arduino works for a long period of time..!!

 

Thanks in advance.. image

  • Sign in to reply
  • Cancel

Top Replies

  • alanwood
    alanwood over 13 years ago +1
    Hi, Are you building your own shield to be mounted on the Arduino? Your circuitry should be able to get enough current from the pins on the Arduino. If in doubt, do a worst case calculation for current…
Parents
  • alanwood
    0 alanwood over 13 years ago

    Hi,

     

    Are you building your own shield to be mounted on the Arduino? Your circuitry should be able to get enough current from the pins on the Arduino. If in doubt, do a worst case calculation for current draw and see if it exceeds the Arduino specifications. Here is a link on ways to destroy an Arduino:  http://ruggedcircuits.com/html/ancp01.html

    http://ruggedcircuits.com/html/ancp01.htmlIt advises that you shouldn't power your own circuits from the Vin pin of the Arduino.

     

    Here is a link to a ruggedized Arduino: http://ruggedcircuits.com/html/ruggeduino.html

     

    Hope you have fun with your design.

     

    Regards,

    Alan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • alanwood
    0 alanwood over 13 years ago

    Hi,

     

    Are you building your own shield to be mounted on the Arduino? Your circuitry should be able to get enough current from the pins on the Arduino. If in doubt, do a worst case calculation for current draw and see if it exceeds the Arduino specifications. Here is a link on ways to destroy an Arduino:  http://ruggedcircuits.com/html/ancp01.html

    http://ruggedcircuits.com/html/ancp01.htmlIt advises that you shouldn't power your own circuits from the Vin pin of the Arduino.

     

    Here is a link to a ruggedized Arduino: http://ruggedcircuits.com/html/ruggeduino.html

     

    Hope you have fun with your design.

     

    Regards,

    Alan