Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Due capability to transmit live videos from IP camera or Web Camera?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 415 subscribers
  • Views 475 views
  • Users 0 members are here
  • hardware
  • embedded
  • camera
  • arduino_due
  • arduino
Related

Arduino Due capability to transmit live videos from IP camera or Web Camera?

e14 Contributor
e14 Contributor over 13 years ago

I am planning to implement an embedded server using Arduino Due Which needs to control a Robotic Arm. The IP camera is needed to monitor the Robotic Arm. The robotic arm needs to be controlled from a remote location far away, so need to send live videos to the remote location.

So is it possible to transmit live video using the Arduino Due through internet using Arduino Ethernet Shield???

I wish to use a webcam/IP Camera.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 13 years ago

    Hi Ron,

     

    It's not easy, because the Arduino Due has only 96kbyte RAM, but a single video frame (even at a low res) may exceed that. Plus, it doesn't run Linux so there are no convenient libraries of code available to compress and also to stream the video. Today, it may be better to use RPI and camera accessory, or the BBB with the camera cape or a webcam.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 13 years ago

    Hi Ron,

     

    It's not easy, because the Arduino Due has only 96kbyte RAM, but a single video frame (even at a low res) may exceed that. Plus, it doesn't run Linux so there are no convenient libraries of code available to compress and also to stream the video. Today, it may be better to use RPI and camera accessory, or the BBB with the camera cape or a webcam.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer