Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Sketch Question???
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 416 subscribers
  • Views 419 views
  • Users 0 members are here
  • multiple
  • byte
  • virtual
  • loop
  • rc
  • sketch
  • car
  • char
  • digits
  • receiver
  • transmitter
  • wire
  • and
  • for
  • rf
  • array
  • arduino
Related

Arduino Sketch Question???

fechrxy
fechrxy over 13 years ago

Hey, so i am writing a sketch for an rc car. I am using one of those cheap five dollar rf transmitter and receiver modules and am using virtual wire library in my sketch. I had gotten it to when i hit one of the four buttons, the remote control would wirelessly tell one of the two motors which direction to turn. However i cannot seem to figure out how to allow the car to multi task, for example turn right while going forward. I found that i needed to send two bytes at a time the first telling motor A what to do and the second telling motor B what to do. The wireless data is handled in a for loop when received thus meaning it is in an array. So i geuss i am stuck the two sketches below (transmitter and receiver) will happily control the direction of the first motor but just doesn't seem to work with the second. I know i did a terrible job of explaining so if needed i can provide additional information. Thanks so much.    (I attatched the files below)

 

 

 

TRANSMITTER

 

// you must download and install the VirtualWire.h

// to your hardware/libraries folder

#include <VirtualWire.h>

 

 

const int Enable_Motor_A = 9;

const int P1_Motor_A = 11;

const int P2_Motor_A = 13; 

 

 

const int Enable_Motor_B = 10;

const int P1_Motor_B = 5;

const int P2_Motor_B = 6;

 

 

byte msg[1];

 

 

void setup()

{

   Serial.begin(9600);

  pinMode(6, INPUT);

    pinMode(13, INPUT);

    pinMode(8, INPUT);

    pinMode(9, INPUT);

   

  

    vw_setup(2000);

    vw_set_tx_pin(7);

}

 

 

void loop()

{

    

 

 

  msg[0] = '0';

      msg[0] = '0';

    if(digitalRead(13) == HIGH) {

      msg[0] = '1';

    }

    

   

    else if(digitalRead(6) == HIGH) {

      msg[0] = '2';

    } 

   

    if(digitalRead(8) == HIGH) {

      msg[1] = '3';

    }

    

   

    else if(digitalRead(9) == HIGH) {

      msg[1] = '4';

    }

  

   

 

 

 

   vw_send(msg, 1);

  

   vw_wait_tx();

 

   

}

 

 

 

RECEIVER

 

#include <VirtualWire.h>

 

 

const int Enable_Motor_A = 9;

const int P1_Motor_A = 12;

const int P2_Motor_A = 13; 

 

 

const int Enable_Motor_B = 10;

const int P1_Motor_B = 5;

const int P2_Motor_B = 6;

 

 

 

 

byte buf[1];

byte buflen;

void setup()

{

  buflen = 1;

 

 

  pinMode(Enable_Motor_A, OUTPUT);  //Declares the three 'Motor A' pins as outputs.

  pinMode(P1_Motor_A, OUTPUT);

  pinMode(P2_Motor_A, OUTPUT);

  

  pinMode(Enable_Motor_B, OUTPUT);  //Declares the three 'Motor B' pins as outputs.

  pinMode(P1_Motor_B, OUTPUT);

  pinMode(P2_Motor_B, OUTPUT);

 

  digitalWrite(Enable_Motor_A, LOW); 

  digitalWrite(P1_Motor_A, LOW);

  digitalWrite(P2_Motor_A, LOW);

  

  digitalWrite(Enable_Motor_B, LOW); 

  digitalWrite(P1_Motor_B, LOW);

  digitalWrite(P2_Motor_B, LOW);

 

  vw_setup(2000);

  vw_set_rx_pin(7);

  vw_rx_start();

 

  

 

}

 

 

 

 

void loop()

{

  uint8_t buflen = VW_MAX_MESSAGE_LEN;

  uint8_t buf[buflen];

 

  if (vw_get_message(buf, &buflen))          

  {

    for(int i = 0;i < buflen;i++)           

  { 

  if (buf[0] == '1')                                //FORWARDS BUTTON

   {

    digitalWrite(P2_Motor_A, LOW);

    digitalWrite(P1_Motor_A, HIGH);

    analogWrite(Enable_Motor_A, 255);}

 

 

  else if (buf[0] == '2')                         //BACKWARDS BUTTON

  {

    digitalWrite(P1_Motor_A, LOW);

    digitalWrite(P2_Motor_A, HIGH);

    analogWrite(Enable_Motor_A, 255);}

 

 

  

 

 

  else                                            //NIETHER BUTTONS

   { 

    digitalWrite(P1_Motor_A, LOW);

    digitalWrite(P2_Motor_A, LOW);

    digitalWrite(Enable_Motor_A, LOW);}

    

 

 

 

 

  if (buf[1] == '3')                              //RIGHT BUTTON

  {

    digitalWrite(P2_Motor_B, LOW);

    digitalWrite(P1_Motor_B, HIGH);

    analogWrite(Enable_Motor_B, 255);}

    

  else if (buf[1] == '4')                         //LEFT BUTTON

  {

    digitalWrite(P1_Motor_B, LOW);

    digitalWrite(P2_Motor_B, HIGH);

    analogWrite(Enable_Motor_B, 255);}

   

  else                                            //NIETHER BUTTONS

   {                      

    digitalWrite(P1_Motor_B, LOW);

    digitalWrite(P2_Motor_B, LOW);

    digitalWrite(Enable_Motor_B, LOW);}

  }}

 

 

 

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1 +1
    In TRANSMITTER: msg[0] = '0'; msg[0] = '0'; one of these should set msg[1]. Edited to add: In RECEIVER, you have: for(int i = 0;i < buflen;i++) but then you don't reference 'i'. Instead you say for example…
  • mcb1
    0 mcb1 over 13 years ago

    Tony

    I'd be slightly more inclined to help, if you answered or acknowledged the other questions you pose.

     

    Good luck.

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    In TRANSMITTER:

    msg[0] = '0';

          msg[0] = '0';

     

    one of these should set msg[1].

     

     

    Edited to add:

    In RECEIVER, you have:

                    for(int i = 0;i < buflen;i++)

     

    but then you don't reference 'i'.  Instead you say for example:

          if (buf[0] == '1')   

    referencing buf[0] rather than buf[i], which I don't think is what you want.