Arduino
  • Products
  • More
Arduino
Arduino Forum Serial array problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 416 subscribers
  • Views 932 views
  • Users 0 members are here
Related

Serial array problems

tabarus12
tabarus12 over 13 years ago

Hi guys, Im having problems storing arrays of data from the serial input of the arduino, I made a program to read the data and print back the array ordered but it does not seem to work.

 

It prints this.

 

I recived: 1-0-0-0-0-0-0-0-

I recived: 2-0-0-0-0-0-0-0-

I recived: 3-0-0-0-0-0-0-0-

 

When it should be printing this.

 

I recived: 1-2-3-0-0-0-0-0-

 

Can anyone tell me where Im wrong?

 

Here is the code, the program reads it ok just does not store it correctly.

 

int d[8];

int b = 0;

 

void setup() {

  Serial.begin(9600);

}

void loop() {

  b = 0;

  for(b = 0; b < 8; b++) {

    d[b] = 0;

  }

  b = 0;

  while(Serial.available() > 0) { //Verifies serial byte ready

    Serial.println(""); //New line

    Serial.print("I recived: "); //Prints the start mesage

    for (b = 0; b < 8; b++) { //Increase array location

      while(Serial.available() > 0) {  //Verifies serial byte ready

        d[b] = Serial.read() - 48; //Stores data on array location

      }

      Serial.print(d[b]); //Prints data array location

      Serial.print("-"); //Separator

    }

  }

}

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +1
    Ha, we had a race condition.
  • tabarus12
    tabarus12 over 13 years ago +1
    Found the issue, the for was running too fast, problem solved with a 1 millisecond delay on the for loop to allow the serial interface to set next value. Any how thanks for the tips Ill try them too.
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

          while(Serial.available() > 0) {  //Verifies serial byte ready

            d[b] = Serial.read() - 48; //Stores data on array location

          }

     

    I think you want an "if" instead of "while".

    The "while" causes each value that is read to be stored into

    the same location, overwriting the previous value, because

    b isn't incremented within the "while" loop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    Ha, we had a race condition.  image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    Ha, we had a race condition.  image