Arduino
  • Products
  • More
Arduino
Arduino Forum Analog input 'Tare/Zero' Weight Function
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 2957 views
  • Users 0 members are here
Related

Analog input 'Tare/Zero' Weight Function

e14 Contributor
e14 Contributor over 13 years ago

Hi, I am currently working with a load cell amplifier, the output I have taken to Anal Input A0, I need to 'Tare/Zero' the low weight input value, and subtract that value from further

weighed values.

 

I would like to carry out the 'Tare/Zero' via a push button (one shot) which would store the zero value until the power supply is removed.

 

I would also like to display the zero weight via the 'Monitor' function, in order to proove the 'Tare' function is working every time.

 

I have completed the weighing code of the project. but I am completely stumped on the 'Tare/Zero' stage, I can't find an example of storing or one shot code.

 

I hope you can help to enable me to go forward with the project.

 

Regards,

 

Gordon

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor +1
    Gordon That result is a different problem than the impression you gave from you first post..... To prove the loadcell is working, try loading and running the example AnalogInOutSerial. This should prove…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1 +1
    Hi Mark, Hurray, I have found the problem!! I needed to create a new register 'int ZeroVal' as shown. then later the subtraction worked! I have improved the HMI monitor layout and it looks great, all I…
Parents
  • mcb1
    0 mcb1 over 13 years ago

    Gordon

    Without seeing your code I can't offer the exact code but something along these lines should work.

     

    Detect 'zero' button

    Read analog and store in a variable (ie int ZeroValue = 0; // value to store zero reading)

     

    Whenever you read the load cell, you subtract the ZeroValue from the reading

     

    Detect the 'monitor' button

    display or print the ZeroValue rather than the load cell reading

     

    This will remain until the micro is reset, either by power, reset button or upload.

     

    Good luck

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    Hi Mark,

     

    Thank you for your early feedback, you described it exactly how I would do it in PLC terms, I am new to Arduino so I am struggling with the code structure, I feel your suggestion will work, I will need to trial a few sketches and then import the working code into my current project.

     

    Best wishes,

     

    Gordon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    Hi Mark,

     

    Thank you for your early feedback, you described it exactly how I would do it in PLC terms, I am new to Arduino so I am struggling with the code structure, I feel your suggestion will work, I will need to trial a few sketches and then import the working code into my current project.

     

    Best wishes,

     

    Gordon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    int loadCellPin = 1;

    int tareButtonPin = 8;

    int currentWeight = 0;

    int taredWeight = 0;

     

    void loop() {

      //do some math to convert anaglogRead(loadCellPin) to a weight

      currentWeight = //results of that math;

     

      //check if the tare button is pushed, to see if it needs to store a value.

      if (digitalRead(tareButtonPin) == HIGH) {

        taredAmt = anaglogRead(loadCellPin);

      }

     

      //do the math to convert taredWeight from 0-1023 to a weight

     

      //i assume you'll have some sort of lcd code setup

      lcd.print("Weight: ");

      lcd.print(currentWeight - taredWeight);

    }

     

    This is what you need on a very basic level, but without any specifics I cant help too much more.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi,

     

    Thanks for the assistance, I would like to send my code to you to check it over, I am only a beginner and it has been trial and error so far.

     

    Basically I want to store a weight to an SD card shield which I have setup ok, but the tare function has stumped me!

    I have 2 buttons, button 1 is the Tare/Zero, Button 2 is the 'take weigh sample' button.

     

    I have setup to write to monitor and I can display the Tare weight when button 1 is pressed, when Button 2 is pressed it displays a scaled value in Pounds/Ounces, my problem is I cant get the subtraction of the Tare weight to work.

     

    I would appreciate any help you could give me.

     

    How can I send you the code?

     

    Regards,

     

    Gordon