Arduino
  • Products
  • More
Arduino
Arduino Forum what objects to receive OSC bundles via SLIPSerial stream in MAX msp
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 667 views
  • Users 0 members are here
  • communications
  • max
  • msp
  • slipserial
  • osc
  • serial
  • arduino
Related

what objects to receive OSC bundles via SLIPSerial stream in MAX msp

e14 Contributor
e14 Contributor over 13 years ago

Hello!

 

I am sending OSC bundles over SLIPSerial from the arduino, and trying to recieve them in Max msp and then route the messages to perameters in Max.

 

In the Arduino code i am creating a OSC bundle and adding two messages to it, the first sets a directory of "/analog/ch1" and then reads anolog pin 0 to the end of that message, then the 2nd message sends "/analog/ch2" and reads analog pin 1 to the end.

 

then i send the the bundle over SLIP serial.

 

 

#include <OSCBundle.h>

#include <OSCMessage.h>

 

#include <SLIPEncodedSerial.h>

SLIPEncodedSerial SLIPSerial(Serial);

 

void setup() {

 

Serial.begin(38400);

}

 

void loop(){

 

  OSCBundle bndl;

  bndl.add("/analog/ch1").add(analogRead(0));

  bndl.add("/analog/ch2").add(analogRead(1));

  bndl.send(SLIPSerial);

 

 

}

 

 

I can see in the serial monitor that the serial messages are being send but i am having trouble receiving the messages in Max MSP

 

There are a number of objects included the External objects from CNMAT, but i can't seam to get any of them to work in conjunction with each other.

 

 

does anyone know how to get this OSC going over serial? or should i just get the ethernet sheild and communicate over UDP?

 

 

thanks!!

 

steve

  • Sign in to reply
  • Cancel
Parents
  • billabott
    0 billabott over 13 years ago

    http://cnmat.berkeley.edu/events   on sep 13th 2013

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    Hey Bill,

     

    thanks a lot for posting this workship, It looks really interesting and I plan on attending!

     

    in responce to my earlyer post, i have tried to get the SLIPencodedserial library working in conjuction with the Max MSP objects, but i have had no luck. Do to a time contraint for my class project i had to use the Maxuino / Firmata solution Although this worked, however this is exteremely in effeicient and not always reliable. In the future i hope to tackle the oscuino CNMAT libraries! thanks again for your input

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    Good for you, but it seems that I saw a statement on the site that Arduino and the libraries were not up to the task. 

     

    On the other hand, you should know that the master puppeteer, Mark Setrakian from ILM, is using arduinos for some of his creature creations and uses MAX for rhythmic servo actuation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    Good for you, but it seems that I saw a statement on the site that Arduino and the libraries were not up to the task. 

     

    On the other hand, you should know that the master puppeteer, Mark Setrakian from ILM, is using arduinos for some of his creature creations and uses MAX for rhythmic servo actuation.