Arduino
  • Products
  • More
Arduino
Arduino Forum what objects to receive OSC bundles via SLIPSerial stream in MAX msp
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 669 views
  • Users 0 members are here
  • communications
  • max
  • msp
  • slipserial
  • osc
  • serial
  • arduino
Related

what objects to receive OSC bundles via SLIPSerial stream in MAX msp

e14 Contributor
e14 Contributor over 13 years ago

Hello!

 

I am sending OSC bundles over SLIPSerial from the arduino, and trying to recieve them in Max msp and then route the messages to perameters in Max.

 

In the Arduino code i am creating a OSC bundle and adding two messages to it, the first sets a directory of "/analog/ch1" and then reads anolog pin 0 to the end of that message, then the 2nd message sends "/analog/ch2" and reads analog pin 1 to the end.

 

then i send the the bundle over SLIP serial.

 

 

#include <OSCBundle.h>

#include <OSCMessage.h>

 

#include <SLIPEncodedSerial.h>

SLIPEncodedSerial SLIPSerial(Serial);

 

void setup() {

 

Serial.begin(38400);

}

 

void loop(){

 

  OSCBundle bndl;

  bndl.add("/analog/ch1").add(analogRead(0));

  bndl.add("/analog/ch2").add(analogRead(1));

  bndl.send(SLIPSerial);

 

 

}

 

 

I can see in the serial monitor that the serial messages are being send but i am having trouble receiving the messages in Max MSP

 

There are a number of objects included the External objects from CNMAT, but i can't seam to get any of them to work in conjunction with each other.

 

 

does anyone know how to get this OSC going over serial? or should i just get the ethernet sheild and communicate over UDP?

 

 

thanks!!

 

steve

  • Sign in to reply
  • Cancel
Parents
  • billabott
    0 billabott over 13 years ago

    http://cnmat.berkeley.edu/oscuino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago

    http://cnmat.berkeley.edu/oscuino