I'm new at using the arduino and I need some help I have been asked to design a arduino with wifi and using a 3 wire temperature probe capable of measuring down to -90 degrees C and a PC program capable of receiving the data and storing it in a file and activating an alarm when the temperature goes under or over set limits. preferable also to have a display on board for the temperature and the ability to calibrate the probe
Q1. What would the best arduino to use
Q2. Is there a kit for 3 wire probes I have had a look and all I can find is 1 wire
Q3. Would it be able to have more than one device running at the same time with no conflicts
Q4. Would anyone be able to design the device for me I am willing to negotiate on the price
Note the device is to be used in a bio storage freezer but I would like the adaptability to use it in the lab fridges as well