Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino code help.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 1179 views
  • Users 0 members are here
  • buttons
  • led
  • code
  • arduino
Related

Arduino code help.

e14 Contributor
e14 Contributor over 12 years ago

I'm in the middle of an arduino project and I need help with the push buttons I'm using.

 

I need to be able to push a button that tells the arduino to set the LED value to 1 but not have the LED light up,

I also need there to be another button that makes all the push buttons that HAVE BEEN PRESSED light up.

 

Any help with the code or any resources that can help me are very much appreciated!

 

If this is not possible please tell me!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    The idea is to have a project box with about 10 buttons on the project box and little LEDs next to them, wherever the LEDs are placed, there will be pieces of paper indicating what each button represents…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Just explain me your project, I will try to help you. I can't understand what you really want  with your explanation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The idea is to have a project box with about 10 buttons on the project box and little LEDs next to them, wherever the LEDs are placed, there will be pieces of paper indicating what each button represents next to the LEDs . The box would also have 2 buttons on the side of the project box, one would be used to turn on the leds that had their corresponding buttons pushed and the other

    would reset the system so it could be used with different combonations.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    That is a an easy code to program, you just have to set each push button to set a value "ON" on each correspondent LED.

     

    I don't understand what you want to do with the other two push buttons.

     

    I will not make the code for you since you are here to learn, so write your code and I will be glab to help you with any errors and give you any advise if you need.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    That is a an easy code to program, you just have to set each push button to set a value "ON" on each correspondent LED.

     

    I don't understand what you want to do with the other two push buttons.

     

    I will not make the code for you since you are here to learn, so write your code and I will be glab to help you with any errors and give you any advise if you need.